Skip to main content
Cubenator
Associate
Mar 17, 2022 10:33 AM UTC
Question

CubeMonitor-RF - How to change TX Interval for RF-Tests?

Hello

I am able to succesfully run the "RF Tests" using a nucleo board (STM32WB55) and a dongle, both connected on the same computer via virtual com port.

Now I'd like to change some parameters for the test, e.g. the TX interval on the nucleo board.

I thought I can do this via the ACI commands HCI_LE_SET_ADVERTISING_PARAMETERS.

However, if I change the minimum and maximum advertising interval, nothing changes. I run the test for about 5s and I get about 8000 packets on the receiver which corresponds to the 0.625 ms interval. If I change the intervals, I still get 8000 packets.

What do I am missing here?

This topic has been closed for replies.

1 reply

Remy ISSALYS
ST Technical Moderator
Mar 23, 2022 4:54 PM UTC

Hello,

Can you tell us which command sequence are you using and how you count the packets?

Best Regards