Question
Consumption current is raised when wake-up from stop mode
Hello Users,
I test BLE with low power.
measured current is 250uA when pcb power was on.
After 10sec(INIT Advertising timeout) enter stop mode and measured current is 4uA.
If EXTI1 detect raising edge, wake up from stop mode. set system_clock_config and normally act re-advertising. but measured current is 2.5mA. I expected to wake up in the same condition as the first time.
Which document can I refer to to to solve this?
I attached my project in google drive link.
https://drive.google.com/file/d/1hlZh2q2eH-TDoElUJ05OjvQzDDG9fWRw/view?usp=sharing
Best Regard.