Concurrent peripheral BLE connections seems to break from stack version v1.21.0
- 0 replies
- 8 views
Hi,
I am having some issues with concurrent peripheral connections when using the stm32wb5x_BLE_Stack_full_fw version 1.21.0.
I created a minimal project using CubeMX according to STM32WB Bluetooth® LE - STM32CubeMX Application Conception, targeting an STM32WB5MM-DK board with the following modifications:
- Targeted to v1.20.0 repository.
- RFWKP clock set to HSE/1024.
- Added restarting advertising until 2 connections are established.
- Added advertising at the shortest connection interval of any existing connection (or default if there are no existing connections)
The firmware for this is attached to this post.
When running this on the STM32WB5MM-DK with stm32wb5x_BLE_Stack_full_fw version 1.20.0 I can successfully connect 2 central devices to it, however if I change the stack version to 1.21.0 the second central device connects and immediately disconnects.
In both scenarios it is the same to central devices connecting.
- iOS device using BLEHero App (Connection interval 30mS, timeout 720mS)
- nRF Connect for Desktop Bluetooth Low Energy Standalone (Connection interval 30mS, timeout 1000mS)
No matter which order the centrals connect, it is always the second connection that drops.
Any help would be greatly appreciated.