Question
Class C downlink not working in STM32WL55JC2.
- My STM32WL55JC2 is programmed with the example code for Lora End Node given in the SDK v1.3.0.
- Class_A is enabled by default and working properly i.e. receive window of the MCU opens only after the periodic uplink.
- When the class is set to Class_C in the LmHandlerConfigure(&LmHandlerParams) function, it still functions like a Class_A device.
- I also tried to change the class later in the join request, but that was also unsuccessful.
Any suggestions?