Skip to main content
Associate III
May 21, 2024 7:31 PM UTC
Question

Choose Interrupt or DMA for UART and SPI slave for minimum cell energy consumption

Would Interrupt or DMA consume less cell energy (need months of cell life)

for UART and SPI for STM32WLE5JCI6?

SPI links with slave sensor chip. Data volume 100 bytes per second.

STM32 master SPI clock can choose 2 to 10 MHz as slave sensor specification.

MCU stays in power saving mode for most time.  Only wake up briefly to do simple processing and back to power saving mode ASAP.

Use Sequencer in utility of HAL WL firmware library

For these HAL library functions.

(+) HAL_UART_Transmit_IT()

(+) HAL_UART_Receive_IT()

(+) HAL_UART_Transmit_DMA()

(+) HAL_UART_Receive_DMA()

HAL_SPI_Transmit_IT()

HAL_SPI_Transmit_DMA()

HAL_SPI_Receive_IT()

HAL_SPI_Receive_DMA()

 

Many thanks

 

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
May 21, 2024 8:05 PM UTC

Hello @David_ 

If you are looking for an Ultra-low-power application on the STM32WL, i suggest you to take a look at the AN5568. For your specific questions, i suggest you to test each implementation and measure the crurent consumption to assume the best implementation.

Best Regards.

STTwo-32 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.