Skip to main content
Associate II
Aug 25, 2025 3:27 PM UTC
Solved

Cannot run any example on Nucleo-WB55RG board

Hello @STTwo-32,

I was having the same issue and pressing the "start wireless stack" button did the trick for me. 

I was assuming after flashing the FUS & BLE Stack firmware, is that the CPU2 would be up and running already. So, does this mean that we need to manually start the CPU2 by pressing the button? 

Thanks!

This post is created based on a comment for this post.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 25, 2025 7:27 PM UTC

Hello @Jopail12 

After the installation of a wireless stack, by default it starts running just after installation without the need for any user action. But if the user application sends two consecutive FUS_GET_STATE commands, the wireless stack boots again on FUS. From a user perspective, the wireless stack is installed but not running (FUS is running).

In that case, it is possible to launch the wireless stack execution by sending the FUS_START_WS command. This command switches from the Arm® Cortex®-MO+ execution to the wireless stack, and results in at least one system reset. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 25, 2025 7:27 PM UTC

Hello @Jopail12 

After the installation of a wireless stack, by default it starts running just after installation without the need for any user action. But if the user application sends two consecutive FUS_GET_STATE commands, the wireless stack boots again on FUS. From a user perspective, the wireless stack is installed but not running (FUS is running).

In that case, it is possible to launch the wireless stack execution by sending the FUS_START_WS command. This command switches from the Arm® Cortex®-MO+ execution to the wireless stack, and results in at least one system reset. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Jopail12Author
Associate II
Aug 26, 2025 4:00 AM UTC

Hello @STTwo-32,

Thanks for the clear explanation!

Appreciate it! 

Regards,
Jopail