Skip to main content
Visitor
Nov 13, 2026 10:23 AM UTC
Solved

Cannot change PA level above +2.6dBm in Cube monitor RF for STM32WBA54 (48pin QFN)

PA level 28 is max.
​​​​​​

Hi!
I’m using a custom made board for STM32WBA54 and the Direct test mode from CubeMX and CubeIDE (STM32Cube FW_WBA V1.10.0). 
We have tried to set the board in high power mode in CubeMx and in CubeRF change PA level but it does not work. Not sure what I’m doing wrong here?
BR
johannes

Laurent LOUAZON
Laurent LOUAZONBest answer
ST Employee
Nov 16, 2026 8:52 AM UTC

Hello,

Plase have a look at below wiki page.
STM32WBA Bluetooth® LE RF Output Power Configuration - stm32mcu

As you can see, there is a matter of HW configuration but this is mainly if using a SMPS version of STM32WBA.
In your case, as using STM32WBA54 (no SMPS), VDDRFPA should be supplied by Vdd so no reason for ,not having the max output power.

You should look at at power table configuration.

Depending power table called, you may be limited to 2.6dBm.
if willing to have the max output power, please call power table 0.

 

Regards
Laurent
 

2 replies

JooMAuthor
Visitor
Nov 13, 2026 10:58 AM UTC

HCI_LE_READ_TRANSMIT_POWER reports −20/+10 dBm and levels above 0x1C are accepted
ACI_HAL_SET_TX_POWER_LEVEL with 0x1F, which should give about +6 dBm (5.6 dBm on ST’s board). Event status gives 0x00 so it should be OK?
So it seems like it works, it is just that the table in RF test is limited to +2.6dBm, maybe that is by design?
BR
Joom

Laurent LOUAZON
Laurent LOUAZONBest answer
ST Employee
Nov 16, 2026 8:52 AM UTC

Hello,

Plase have a look at below wiki page.
STM32WBA Bluetooth® LE RF Output Power Configuration - stm32mcu

As you can see, there is a matter of HW configuration but this is mainly if using a SMPS version of STM32WBA.
In your case, as using STM32WBA54 (no SMPS), VDDRFPA should be supplied by Vdd so no reason for ,not having the max output power.

You should look at at power table configuration.

Depending power table called, you may be limited to 2.6dBm.
if willing to have the max output power, please call power table 0.

 

Regards
Laurent