Skip to main content
Associate
Jul 5, 2025 4:47 PM UTC
Solved

Can we power STM32WB0 from two external voltage sources?

We would like to power the VDD33 domain of an STM32WB0 device (STM32WB05KZ) from an external 3.3V source and the other domains from an external 1.8V source. In theory, it should be possible - by supplying 1.8V to VDDSD in SMPS BYPASS mode, or directly to VFBSD in SMPS OFF mode. However, it is not clear if the SMPS' input (VDDSD) is isolated from VDDIO (the power diagram in the datasheet shows there is a connection). Please clarify if it is possible to use the described configuration.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 25, 2025 9:42 AM UTC

Hello @maxter 

VDDSD has a dedicated ESD protection (no diode connected between VDDSD and VDD).

Yes, it is possible to supply VDDSD with 1.8V and VDD with 3.3V. When the SMPS is OFF (no inductor between VLXSD and VFBSD) VFBSD pin needs to be supplied with 1.8V and the rest of VDD at 3.3V (it's better to connect VDDSD to 3.3V as well).

I suggest supplying the whole device with 1.8V without SMPS, since there are not significant benefits in using different supplies for our device.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Aug 25, 2025 9:42 AM UTC

Hello @maxter 

VDDSD has a dedicated ESD protection (no diode connected between VDDSD and VDD).

Yes, it is possible to supply VDDSD with 1.8V and VDD with 3.3V. When the SMPS is OFF (no inductor between VLXSD and VFBSD) VFBSD pin needs to be supplied with 1.8V and the rest of VDD at 3.3V (it's better to connect VDDSD to 3.3V as well).

I suggest supplying the whole device with 1.8V without SMPS, since there are not significant benefits in using different supplies for our device.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.