Question
Can the TSC be configured to support more than one active shield?
Our application has two touch sensors surrounded by a shield and an additional independent sensor surrounded by a separate shield. The first pair of sensors are connected to TSC groups 1 and 3. The other sensor uses groups 4 and 6. Groups 1 and 4 connect to the active shields. Unfortunately, CubeMX 6.3.0-RC5 does not allow more than one active shield to be selected. Is this due to a HW constraint (we're using the STM32WB5MMG) or a CubeMX error? If this configuration is supported by the TSC, what source code changes are required to work around CubeMX?