Skip to main content
Visitor II
Aug 9, 2024 12:18 PM UTC
Question

Can`t transmit a hex number via LoRa with nucleo-wl55jc1. Nonce joining problem and transmission help.

I need to program the Nucleo-wl55jc1 for work to send data via LoRa. I followed the stm tutorials and connected successfully to the lora chirpstack server. The first connection worked fine, but when reseting the nucleo, it gives some nonce error because I think the nonce value is not storred correctly in flask memory upon successful join. I searched 2 days on the internet and looking trouth the code, but unsuccessfull. Now, to take a break from this, I want to send data on the first successful join, after reseting server nonce. I found the ping pong example, but I don`t understand it well, and I want sonething like a function to send hex data via LoRa. After I have that function made, I can decode the I2C data from another sensor and send it`s data via lora once every 8h.

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Aug 28, 2024 10:15 AM UTC

Hello @Tonikiller10000 

First, The PingPong application is not a LoRaWAN application. If you are looking for a LoRaWAN application to send data From I2C to Your board and then to a LoRaWAN network, please follow the implementation available on the videos 3,4 and 5 of this Playlist.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.