Skip to main content
Associate
Jan 5, 2026 12:52 PM UTC
Solved

Can't Program or erase NUCLEO-WL55JC1

I have just received 2 NUCLEO-WL55JC1. Upon connecting either one of them via I see The Red (main power) and green LEDs on. The other thre are flashing alternatively (red, orange, blue). I haven't changed the default jumper settings.
The following debug probes were found:
[0]: STLink V3 -- 0483:3754:0026003A3234510A33353533 (ST-LINK)

12:21:32 : STM32CubeProgrammer API v2.21.0 | Linux-64Bits
12:21:46 : UR connection mode is defined with the SWrst reset mode
12:21:46 : ST-LINK SN : 0026003A3234510A33353533
12:21:46 : ST-LINK FW : V3J16M8
12:21:46 : Board : NUCLEO-WL55JC
12:21:46 : Voltage : 3.24V
12:21:46 : Unable to get core ID
12:21:46 : No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
12:21:46 : ST-LINK SN : 0026003A3234510A33353533
12:21:46 : ST-LINK FW : V3J16M8
12:21:46 : Board : NUCLEO-WL55JC
12:21:46 : Voltage : 3.23V
12:21:46 : Error: Unable to get core ID
12:21:46 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

Imen.DBest answer
ST Technical Moderator
Jan 5, 2026 1:03 PM UTC

Hello @mapfumo and welcome to the Community,

To resolve connection errors when connecting and programming the STM32 target board, try the tips described in this article: How to solve connection errors when connecting and programming the STM32 target board

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
Jan 5, 2026 1:03 PM UTC

Hello @mapfumo and welcome to the Community,

To resolve connection errors when connecting and programming the STM32 target board, try the tips described in this article: How to solve connection errors when connecting and programming the STM32 target board

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
mapfumoAuthor
Associate
Jan 5, 2026 1:32 PM UTC

Thank you. That worked.