Skip to main content
RBech.1
Visitor II
Jan 18, 2021 6:04 PM UTC
Question

Can't discover STM32WB55 GATT Server after running p2pServer project from firmware.

Hello,

I am using STM32 Cube Ide and I am just getting started with the STM32 WB55 board. I tried running the p2p Server project from the firmware package but I can't see the board neither on nrf Connect application or ST BLE Sensor app. Does anyone has the same problem ?

This topic has been closed for replies.

1 reply

Remi QUINTIN
ST Technical Moderator
Jan 22, 2021 2:26 PM UTC

​Did you try to load the BLE_p2pServer_reference.hex file located  under the

STM32Cube_FW_WB_V1.10.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pServer\Binary directory.

Then use the ST BLE sensor mobile application  to detect it and connect to it.

This would ensure your board is OK.