Skip to main content
Associate III
Dec 21, 2025 7:28 AM UTC
Solved

Can not flash stm32wb5x_Zigbee_FFD_fw.bin

Hi,

i have a bit of situation here.

I wanted to try a zigbee example from cube mx (On/off ED).

So i first flashed the FUS v2.2.0 on the device.

But now it turns out that i can not flash the desired FW anymore : stm32wb5x_Zigbee_FFD_fw.bin.

It only errors :(

I have the feeling that this FW is not working with FUS 2.2?

If so - I am right that i can not downgrade FUS anymore once it is updated?

 

This basically would mean i wasted hundreds of EURs for those dev boards.

 

Alan PORTEBest answer
ST Employee
Dec 22, 2025 7:46 AM UTC

Hello @Exeu,

I was able to install stm32wb5x_Zigbee_FFD_fw.bin v1.24.0 with FUS 2.2.0 on my Nucleo-WB55RG.
Using STM32CubeProgrammer v2.21.0:

AlanPORTE_0-1766389080716.png
AlanPORTE_1-1766389092842.png

You are getting error message "failed to erase memory", thus I would recommend to check the configuration of your option bytes. Check if there is no RDP / PCROP / Write Protection enabled.

You should have something similar to this:

AlanPORTE_2-1766389362735.png

Best Regards,
Alan Porte
ST MCU Support Team

 

5 replies

ExeuAuthor
Associate III
Dec 21, 2025 7:31 AM UTC

Exeu_0-1766302279959.png

 

Issamos
Super User
Dec 21, 2025 2:28 PM UTC

Hello @Exeu 

It should work fine with the FUS 2.2.0. Are you sure about the starting address you are setting. Are you using the last STM32Cubeprogrammer. If so, could you please share the result of reading the FUS and stack version using the Read FUS Version button on the CubeProgrammer and the error message you are having. Also, what is  the complete part number of your MCU?

Best Regards.

II

ExeuAuthor
Associate III
Dec 21, 2025 4:11 PM UTC

Hi @Issamos 

sure

Here is FUS Info - Before Update

Pre-FW-Upgrade.png

Then the file i have choosen + the correct start address which should be: 0x0809F000 - According to the release notes.

Since i am using the Nucleo board it should be the WB55RG mcu.

Pre-FW-Upgrade_2.png

Then the error:

Error.png

This error does not come when i flash any FUS_v2_only binaries - See the screenshot of my reply above with the List coming from the releasenotes file.

The borad is the following: https://www.st.com/en/evaluation-tools/p-nucleo-wb55.html

Alan PORTEBest answer
ST Employee
Dec 22, 2025 7:46 AM UTC

Hello @Exeu,

I was able to install stm32wb5x_Zigbee_FFD_fw.bin v1.24.0 with FUS 2.2.0 on my Nucleo-WB55RG.
Using STM32CubeProgrammer v2.21.0:

AlanPORTE_0-1766389080716.png
AlanPORTE_1-1766389092842.png

You are getting error message "failed to erase memory", thus I would recommend to check the configuration of your option bytes. Check if there is no RDP / PCROP / Write Protection enabled.

You should have something similar to this:

AlanPORTE_2-1766389362735.png

Best Regards,
Alan Porte
ST MCU Support Team

 

ExeuAuthor
Associate III
Dec 22, 2025 8:24 AM UTC

Hi @Alan PORTE 

I dunno what is the difference from what I tried but it seems to work now.

What is interesting: I tried with the automatic address determination.

This was running through but it also putted the stack on a different address as mentioned in the release notes?

It was up an running then.

After doing this I was also able to flash it with the address which should be the real one..

Have no idea why :face_with_tears_of_joy: