Skip to main content
Yaroslav Vushnevsky
Associate II
Feb 14, 2022 12:56 PM UTC
Solved

Can not enable CFG_DEBUG_TRACE in CubeMX in ZigBee on STM32WB5MM

CFG_DEBUG_TRACE are gray and I can not enable it. All options are the same as in example project for WB55. I can not use example project because I have different MCU. As I understand, bug exists for years, but nobody cares.

This topic has been closed for replies.
Sara BEN HADJ YAHYA
ST Technical Moderator
Feb 15, 2022 3:17 PM UTC

Hello @Yaroslav Vushnevsky​ ,

Thanks for your feedback,

To enable CFG_DEBUG_TRACE, CFG_HW_USART1_ENABLED or CFG_HW_LPUART1_ENABLED must be set as well as CFG_DEBUG_TRACE_UART. The issue comes from the missing CFG_DEBUG_TRACE_UART in CubeMX.

I've raised this issue internally to be fixed as soon as possible. I'll keep you posted with the updates.

Internal ticket number: 122835 (This is an internal tracking number and is not accessible or usable by customers).

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Thanks for your contribution and do not hesitate to raise any issue/ feedback.

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

3 replies

Sara BEN HADJ YAHYA
ST Technical Moderator
Feb 15, 2022 3:17 PM UTC

Hello @Yaroslav Vushnevsky​ ,

Thanks for your feedback,

To enable CFG_DEBUG_TRACE, CFG_HW_USART1_ENABLED or CFG_HW_LPUART1_ENABLED must be set as well as CFG_DEBUG_TRACE_UART. The issue comes from the missing CFG_DEBUG_TRACE_UART in CubeMX.

I've raised this issue internally to be fixed as soon as possible. I'll keep you posted with the updates.

Internal ticket number: 122835 (This is an internal tracking number and is not accessible or usable by customers).

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Thanks for your contribution and do not hesitate to raise any issue/ feedback.

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
FSax
Visitor II
Feb 22, 2022 8:50 AM UTC

Any news about this issue?

Thanks

Sara BEN HADJ YAHYA
ST Technical Moderator
Mar 7, 2022 2:45 PM UTC

Hello @Yaroslav Vushnevsky​ , @FSax​ ,

This issue is fixed in STM32CubeMX latest release.

V6.5.0 is now available under this Link.

Thanks for your contribution.

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.