Skip to main content
KKIM.6
Senior
Jul 6, 2022 7:00 PM UTC
Solved

Can I use SMPS in microcontroller for AC-DC converter?

The STM32WB55 microcontroller have SMPS internally.

 

Can I use it to convert AC power to DC power for the microcontroller?

 

If possible, I want to supply RF inductive charging power directly to the microcontroller.

 

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
Jul 7, 2022 4:04 PM UTC

it tells you that the minimum input is, essentially, zero - so you can't apply AC.

Therefore you would need to provide any rectification externally.

The datasheet also tells you that it is a step-down SMPS, so it wouldn't be able to cope with a rectified AC supply - which drops to zero once (half-wave) or twice (full-wave) per cycle.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

6 replies

KKIM.6
KKIM.6Author
Senior
Jul 6, 2022 10:14 PM UTC

After reading manual, I understood the SMPS is only for power efficiency when Vdd is high enough than 3.3 V. Unfortunately, I think it cannot be used for AC-DC converter...

Andrew Neil
Super User
Jul 7, 2022 8:56 AM UTC

"After reading manual, I understood"

Yes, that is why manufacturers provide datasheet to tell you these things!

Absolute Maximum limits:

0693W00000QKdUxQAL.png 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
KKIM.6
KKIM.6Author
Senior
Jul 7, 2022 1:34 PM UTC

No. My question is whether SMPS in microcontroller can be used for AD-DC converter but, it is not in manual.