Skip to main content
Ajoub.1
Associate II
Aug 21, 2021 1:14 PM UTC
Solved

can I use an external flash and RAM at the same time on STM32wb55

I'm trying to add an external FLASH and RAM to the STM32WB55, but he doesn't have an FMC or FSMC, and all resources a could find related to this subject use the FMC peripheral, there is any way to use the external RAM and FLASH in the same time?

should I use 1 QSPI for both of them?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 21, 2021 2:16 PM UTC

No.

You can only use one, the design is optimized for a QSPI NOR Flash, allows for execute-in-place.

What kind of FLASH/RAM resources does your application need?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 21, 2021 2:16 PM UTC

No.

You can only use one, the design is optimized for a QSPI NOR Flash, allows for execute-in-place.

What kind of FLASH/RAM resources does your application need?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ajoub.1
Ajoub.1Author
Associate II
Aug 21, 2021 2:27 PM UTC

hey, thank you for your reply

I'm looking for an extra 1 Mb of RAM and more than 4 Mb of flash.

what do you think is the solution?

I can optimize the flash because I will use it for a GUI product.

Tesla DeLorean
Guru
Aug 21, 2021 3:42 PM UTC

Mb bit

MB Byte

What do you need 1MB of RAM for?

Perhaps look to a display/controller with it's own on-board frame buffer memory, and which you can communicate with via SPI.

Consider pairing with another MCU with more flash, ram, and capabilities.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..