Skip to main content
satyam9896
Associate III
Sep 26, 2025 1:08 PM UTC
Question

Can BlueNRG-M2SP/M2SA support multiple Central/client connections simultaneously in Peripheral/server role?

Hello,

I am working on a project with STM32 + BlueNRG-M2SP/M2SA and using a custom mobile app  to connect over BLE.

Here is my setup:

  • The BlueNRG-M2SP/M2SA IC module is configured as a Peripheral (Server)  with my stm32l0 mcu.

  • The mobile app scans, finds the advertised name of my hardware, and connects successfully without any pin security.

My question:

  • Is it possible to connect two mobile phones (two Central clients) together to the same BlueNRG-M2SP/M2SA  hardware device when it is in Peripheral/server role?

  • The datasheet mentions “Supports master and slave modes, multiple roles supported simultaneously”. Does this mean multiple Centrals/phones can connect at once, or does it only mean the device can act as both Central and Peripheral (multi-role), but with a limit of one connection per role/same time?

  • If multi-client support in Peripheral/server mode is possible, how can I configure the max number of links in the BlueNRG stack of my stm32l0 firmware code?

Thanks in advance for your clarification.

This topic has been closed for replies.