Skip to main content
PawelM
Associate II
Sep 23, 2020 11:31 AM UTC
Question

BlueST-SDK and STM32WB55 bootloader STM_OTA

Hi

Whether BlueST-SDK tool is compatible with bootloader STM_OTA dedicated to STM32WB55 ?

I using Nucleo STM32WB55 and bootloader from STM (STM_OTA). For update firmware I using for now STM32CubeMonitor-RF and stm32WB USB DONGLE (which is part of nucleo kit). Now I would like to do this in other way - other tools, CLI, scripts...

~/Downloads/BlueSTSDK_Python/blue_st_examples $ sudo python3 example_ble_6.py 
 
##################
# BlueST Example #
##################
 
Scanning Bluetooth devices...
 
Discovery started.
New device discovered: STM_OTA.
Discovery stopped.
 
Connecting to STM_OTA...
Device STM_OTA connected.
Connection done.
 
Features:
No features found.
1) Firmware upgrade
 
Select an action ('0' to quit): 1 
1)node-stm32wb55
 
Select a firmware ('0' to cancel): 1
 
Upgrading firmware...
1
<bound method Node.get_debug of <blue_st_sdk.node.Node object at 0x7647b490>>
none
2
Traceback (most recent call last):
 File "example_ble_6.py", line 327, in main
 upgrade_console.add_listener(upgrade_console_listener)
AttributeError: 'NoneType' object has no attribute 'add_listener'
 
During handling of the above exception, another exception occurred:
 
Traceback (most recent call last):
 File "example_ble_6.py", line 391, in <module>
 main(sys.argv[1:])
 File "example_ble_6.py", line 346, in main
 upgrade_console.remove_listener(upgrade_console_listener)
AttributeError: 'NoneType' object has no attribute 'remove_listener'
Device STM_OTA disconnected.
Exception ignored in: <function Peripheral.__del__ at 0x76572108>
Traceback (most recent call last):
 File "/usr/local/lib/python3.7/dist-packages/bluepy/btle.py", line 630, in __del__
 File "/usr/local/lib/python3.7/dist-packages/blue_st_sdk/node.py", line 555, in disconnect
 File "/usr/local/lib/python3.7/dist-packages/blue_st_sdk/node.py", line 398, in _update_node_status
 File "/usr/lib/python3.7/concurrent/futures/thread.py", line 151, in submit
RuntimeError: cannot schedule new futures after shutdown

This topic has been closed for replies.

1 reply

ttnickb
Associate II
Sep 1, 2023 2:17 PM UTC

I am seeing this same behavior trying to run `BlueST-SDK v1.4.0` under Python 3.10.  I am using the `example_ble_6.py` from master branch ~Nov 2022.

I tried a couple local modifications but can't seem to resolve yet.  Connecting to the STM32WB device works...but then it fails when starting upload.  It seems like something is wrong with `node.py get_debug()` as this is the function returning `None`.

Given there haven't been any recent commits, I'm not sure if the project is supported anymore.  This is too bad because it seems pretty close to working for firmware updates.