Skip to main content
Remi Demers
Associate II
Apr 10, 2025 7:49 PM UTC
Solved

BLUENRG-LPS DMA seems not working

Hi,

Using Wise studio Version: 1.3.1_R Build id: 2023_05 on Linux with the STEVAL-IDB012V1 (BlueRNG-LPS dev. kit). I am trying to make the DMA sending a series of bytes to the lowest byte of the GPIOB output. The goal is to see a binary sequence appear on PB0 and PB1. I filled the buffer "buffer" with values where bit 0 and 1 are changing. Then, I call the two functions depicted below but nothing happens on PB0 and PB1. I already verified that the counter is counting and the GPIO can drive different values on PB0 and PB1. So I think my problem is in the DMA settings.

#define BUFFER_LENGTH 1400
#define PERIOD_50_US 3200 // 50us from 64Mhz timer 16

uint8_t buffer[BUFFER_LENGTH];

void My_GPIO_Settings()
{
 GPIOA->MODER =0x000000A0;
 LL_GPIO_SetPinMode(GPIOB, LL_GPIO_PIN_0, LL_GPIO_MODE_OUTPUT);
 LL_GPIO_SetPinMode(GPIOB, LL_GPIO_PIN_1, LL_GPIO_MODE_OUTPUT);
}

void DMA_Based_Waveform_Settings()
{
	// Setting DMA channel
	MODIFY_REG(RCC->AHBENR, 0, 1); // Enable the clock for DMA and DMAMUX
	LL_DMA_DisableChannel(DMA1, LL_DMA_CHANNEL_8);
	LL_DMA_ConfigAddresses(DMA1, LL_DMA_CHANNEL_8, (uint32_t)buffer, (uint32_t)&GPIOB->ODR, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
	LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_8, BUFFER_LENGTH);
	LL_DMA_ConfigTransfer(DMA1, LL_DMA_CHANNEL_8, LL_DMA_DIRECTION_MEMORY_TO_PERIPH
			 | LL_DMA_MODE_CIRCULAR
												| LL_DMA_PERIPH_NOINCREMENT
												| LL_DMA_MEMORY_INCREMENT
												| LL_DMA_PDATAALIGN_BYTE
												| LL_DMA_MDATAALIGN_BYTE
												| LL_DMA_PRIORITY_VERYHIGH);
	// Setting timer to clock the DMA
	MODIFY_REG(RCC->APB0ENR, 0, 7); // Enable the clock for TIMs
	TIM16->ARR = PERIOD_50_US; // 3200
	TIM16->DIER = 0x100; // Update DMA request enabled

	// Setting the DMA MUX to make TIM16 clock the DMA transfer
	LL_DMAMUX_SetRequestID(DMAMUX1, LL_DMAMUX_CHANNEL_7, LL_DMAMUX_REQ_TIM16_UP);

 // Starting the transfer
	LL_TIM_EnableCounter(TIM16);
	LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_8);
}
This topic has been closed for replies.
Remi Demers
Remi DemersBest answer
Associate II
Apr 18, 2025 1:46 PM UTC

Finally, I found in the reference manual page 5 figure 1 that the DMA is not connected to the GPIO bus. So what I wanted to do is impossible. It would be a nice feature to make this possible.

2 replies

Remi Demers
Associate II
Apr 14, 2025 3:17 PM UTC

MORE DETAILS:

When I call LL_TIM_EnableCounter(TIM16) before LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_8), the later instruction have no effect on the DMA1_CCR8 bit 0 (It is not set). If I call LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_8) first, the enable bit is set, but it is cleared when LL_TIM_EnableCounter(TIM16) is called. As the circular mode is selected this shall not happens. I wonder if there is a limitation in the silicon for what I am trying to do?

Remi Demers
Remi DemersAuthorBest answer
Associate II
Apr 18, 2025 1:46 PM UTC

Finally, I found in the reference manual page 5 figure 1 that the DMA is not connected to the GPIO bus. So what I wanted to do is impossible. It would be a nice feature to make this possible.