Skip to main content
BBlin.1
Associate II
Oct 4, 2022 10:03 AM UTC
Question

BLE_TransparentMode example project on NUCLEO-WB55RG crashes

I am working on the NUCLEO-WB55RG eval board and I try to run the BLE_TransparentMode project provided as example. But when I run the code (without any modification), it doesn't work. The debugging shows that it failed suddenly at MX_APPE_Init main function.

I have successfully flashed the firmware stm32wb5x_BLE_Stack_full_extended_fw.bin at address 0x080C7000.

Other examples works fine (I've tested BLE_Zigbee_Dyn and Zigbee_APS_Router projects)

I use STM32CubeIDE with STM32Cube_FW_WB_V1.14.1 library.

This topic has been closed for replies.

6 replies

Remy ISSALYS
ST Technical Moderator
Oct 5, 2022 7:30 AM UTC

Hello,

BLE_TransparentMode project allows to send ACI commands using STM32CubeMonitor RF tool. Are you able to connect your board to STM32CubeMonitor RF tool or not ?

Best Regards

BBlin.1
BBlin.1Author
Associate II
Oct 5, 2022 10:24 AM UTC

No, STM32CubeMonitor RF tool can't connect to the board ("device not responding")

Remy ISSALYS
ST Technical Moderator
Oct 5, 2022 4:29 PM UTC

Which version of STM32CubeMonitor RF tool are you using ?

BBlin.1
BBlin.1Author
Associate II
Oct 6, 2022 6:18 AM UTC

Version 2.9.1

Remy ISSALYS
ST Technical Moderator
Oct 7, 2022 9:08 AM UTC

Hello,

I'm not able to reproduce your issue, so maybe there is an issue when you have flashed the BLE stack. Can you retry to flash the firmware stm32wb5x_BLE_Stack_full_extended_fw.bin at address 0x080C7000 and then BLE_TransparentMode_reference.hex firmware from v1.14.1 using STM32CubeProgrammer?

Best Regards

BBlin.1
BBlin.1Author
Associate II
Oct 7, 2022 9:27 AM UTC

Same issue : the nucleo board is totally frozen when I run the software. Thank you for your help, I will start my development from another example.

Best regards