Skip to main content
Associate II
Jun 7, 2024 11:38 AM UTC
Solved

BLE transparent mode firmware for STM32WB55VGQ package.

Hello,

Using custom firmware on an Inhouse designed board, the BLE output seems unmodulated as shown in the picture attached. But using the Transparent mode firmware on a Nucleo-Board (controlled via the Cube monitorRF) the modulation seems good (also attached)

So,

1. Is there any option to tune the modulation further other than default ?

2. Can someone provide the Transparent mode firmware for the STM32WB55VGQ package ? This can help in FCC testing.

This picture shows the sidebands when tx is ON on the 1st channel.

rapoorv_0-1717760112870.png

This picture shows there are no sidebands on the Nucleo Board which are coming in the above pic.

rapoorv_1-1717760236541.png

 

This topic has been closed for replies.
rapoorvBest answer
Associate II
Jul 29, 2024 12:55 PM UTC

We tried by just changing the UART pins to the required one within the code and it worked using the Transparent Mode code used for the Nucleo Board.

So we can close this out.

 

15 replies

rapoorvAuthorBest answer
Associate II
Jul 29, 2024 12:55 PM UTC

We tried by just changing the UART pins to the required one within the code and it worked using the Transparent Mode code used for the Nucleo Board.

So we can close this out.

 

Associate II
Jul 29, 2024 3:08 PM UTC

Yes, it worked. We can close the thread.