Skip to main content
romihs
Associate II
Mar 29, 2023 7:30 PM UTC
Solved

BLE & Thread Concurrent project

Is it possible to create a project in CubeMX for a concurrent BLE & Thread application for the STM32WB55?

My attempts so far only allow for either a BLE or a Thread project (not both together).

Thanks

This topic has been closed for replies.
Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Mar 31, 2023 12:01 PM UTC

Hello,

Unfortunately, CubeMX tool doesn't support concurrent mode application.

Best Regards

3 replies

ST Technical Moderator
Mar 30, 2023 2:23 AM UTC

Hello @romihs​ and welcome to the Community :)

An example of concurrent mode (BLE/Thread) is provided in the STM32CubeWB firmware package.

I advise you to have a look at the available applications, which are located under: Projects\P-NUCLEO-WB55.Nucleo\Applications\ directory.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
romihs
romihsAuthor
Associate II
Mar 30, 2023 3:24 PM UTC

Thanks @Imen DAHMEN​

Yes, I am aware of the projects in the STM32CubeWB package.

The reason I was asking was that I would like to start a clean project with both BLE and Thread, and was just wondering if it could be started from CubeMX...

Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Mar 31, 2023 12:01 PM UTC

Hello,

Unfortunately, CubeMX tool doesn't support concurrent mode application.

Best Regards