Skip to main content
BGeor.1
Associate II
Sep 18, 2025 11:10 PM UTC
Solved

BLE_p2pServer Example: Why adding 2 to aPeerToPeerContext.P2PNotifyServerToClientCharHdle

I would like to know why 2 is added to the P2PNotifyServerToClientCharHdle while checking for an attribute handle match in p2p_stm.c file. Later in the same function, 1 is added to P2PWriteClientToServerCharHdle. Is there an implicit assumption made here to add 2 to a notify handle and 1 to a write characteristic handle. 

P2PNotifyServerToClientCharHdle is declared as uint16_t. Why add 2 to an integer for matching to Attr_Handle.

 

 
static SVCCTL_EvtAckStatus_t PeerToPeer_Event_Handler(void *Event)

{

SVCCTL_EvtAckStatus_t return_value;

hci_event_pckt *event_pckt;

evt_blecore_aci *blecore_evt;

aci_gatt_attribute_modified_event_rp0 * attribute_modified;

P2PS_STM_App_Notification_evt_t Notification;



return_value = SVCCTL_EvtNotAck;

event_pckt = (hci_event_pckt *)(((hci_uart_pckt*)Event)->data);



switch(event_pckt->evt)

{

case HCI_VENDOR_SPECIFIC_DEBUG_EVT_CODE:

{

blecore_evt = (evt_blecore_aci*)event_pckt->data;

switch(blecore_evt->ecode)

{

case ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE:

{

attribute_modified = (aci_gatt_attribute_modified_event_rp0*)blecore_evt->data;

if(attribute_modified->Attr_Handle == (aPeerToPeerContext.P2PNotifyServerToClientCharHdle + 2))

{

/**

* Descriptor handle

*/

return_value = SVCCTL_EvtAckFlowEnable;

/**



This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 19, 2025 5:45 PM UTC

Hello @BGeor.1 

I think you should have a look at the description of the ACI_GATT_ADD_CHAR on the part 2.6.4 of the AN5270. On the BLE Core 6.0 spec, we have:

Characteristic descriptors are used to contain related information about the
Characteristic Value. The GATT profile defines a standard set of characteristic
descriptors that can be used by higher layer profiles. Higher layer profiles may
define additional characteristic descriptors that are profile specific. Each characteristic
descriptor is identified by the characteristic descriptor UUID. A client shall support the
use of both 16-bit and 128-bit characteristic descriptor UUIDs. A client may ignore any
characteristic descriptor declaration with an unknown characteristic descriptor UUID. An
unknown characteristic descriptor UUID is a UUID for an unsupported characteristic
descriptor.


Characteristic descriptors if present within a characteristic definition shall follow the
Characteristic Value declaration. The characteristic descriptor declaration may appear
in any order within the characteristic definition. The client shall not assume the order
in which a characteristic descriptor declaration appears in a characteristic definition
following the Characteristic Value declaration. 

Characteristic descriptor declaration permissions are defined by a higher layer profile or are implementation specific. A client shall not assume all characteristic descriptor
declarations are readable.

 

Best Regards.

STTwo-32

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

STTwo-32
ST Technical Moderator
Sep 19, 2025 3:49 PM UTC

Hello @BGeor.1 

The characteristics is made by 2 or 3 handles

  • First handle is the Characteristic itself
  • Second handle is the value of the characteristic
  • If properties is Indicate or notify, a third value is added to manage the descriptor (Write enable or Disable ).

So, that's why the P2P notification needs to add 2.

 

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
BGeor.1
BGeor.1Author
Associate II
Sep 19, 2025 4:26 PM UTC

Hello STTwo-32,

Thank you for the quick reply. Interesting details. I want to understand how handles are managed little bit further. I would assume GATT server stores these handles in an attribute table when we call the following code.

COPY_P2P_NOTIFY_UUID(uuid16.Char_UUID_128);

aci_gatt_add_char(aPeerToPeerContext.PeerToPeerSvcHdle,

UUID_TYPE_128, &uuid16,

2,

CHAR_PROP_NOTIFY,

ATTR_PERMISSION_NONE,

GATT_NOTIFY_ATTRIBUTE_WRITE, /* gattEvtMask */

10, /* encryKeySize */

1, /* isVariable: 1 */

&(aPeerToPeerContext.P2PNotifyServerToClientCharHdle));

 

Above function returns one handle, aPeerToPeerContext.P2PNotifyServerToClientCharHdle. But it

looks like since it is a notify characteristic, there are two more consecutive handles(First

handle +1, First Handle + 2) stored in the attribute table automatically. Is that how it works?

 

Is there a documentation on this behavior. I don't see any description for this behavior

in AN5289. It doesn't look like core 6.0 spec is very clear about the implementation

details of how attribute handles are stored in the table.

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Sep 19, 2025 5:45 PM UTC

Hello @BGeor.1 

I think you should have a look at the description of the ACI_GATT_ADD_CHAR on the part 2.6.4 of the AN5270. On the BLE Core 6.0 spec, we have:

Characteristic descriptors are used to contain related information about the
Characteristic Value. The GATT profile defines a standard set of characteristic
descriptors that can be used by higher layer profiles. Higher layer profiles may
define additional characteristic descriptors that are profile specific. Each characteristic
descriptor is identified by the characteristic descriptor UUID. A client shall support the
use of both 16-bit and 128-bit characteristic descriptor UUIDs. A client may ignore any
characteristic descriptor declaration with an unknown characteristic descriptor UUID. An
unknown characteristic descriptor UUID is a UUID for an unsupported characteristic
descriptor.


Characteristic descriptors if present within a characteristic definition shall follow the
Characteristic Value declaration. The characteristic descriptor declaration may appear
in any order within the characteristic definition. The client shall not assume the order
in which a characteristic descriptor declaration appears in a characteristic definition
following the Characteristic Value declaration. 

Characteristic descriptor declaration permissions are defined by a higher layer profile or are implementation specific. A client shall not assume all characteristic descriptor
declarations are readable.

 

Best Regards.

STTwo-32

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.