Skip to main content
ABasi.2
Senior
Jun 29, 2025 9:00 PM UTC
Solved

BLE_HeartRateThreadX example file ioc not present

Hello!

i'm trying the example BLE_HeartRateThreadX 

but the ioc file is not present in the directory, is that normal? i'm missing it?

 

also the directory arent arranged like a project maked with cube ide

is it possible to have an example that is maked like a cube ide project using the MCU or board selector?

 

thank you!

best reguards

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jul 1, 2025 2:57 PM UTC

Hello @ABasi.2 

The BLE_HeartRateThreadX and the BLE_p2pServerThreadX are not made based on the STM32CubeMX. So, there is not a ThreadX + BLE example for the STM32WB that is based on a .ioc file.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

9 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jul 1, 2025 2:57 PM UTC

Hello @ABasi.2 

The BLE_HeartRateThreadX and the BLE_p2pServerThreadX are not made based on the STM32CubeMX. So, there is not a ThreadX + BLE example for the STM32WB that is based on a .ioc file.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ABasi.2
ABasi.2Author
Senior
Jul 1, 2025 9:08 PM UTC

Hello  STTwo-32

but why? 

there is another example that have a project created with cubeIDE for the same board? that explain the BLE communication

 

thank you!

 

best reguards 

Andrew Neil
Super User
Jul 2, 2025 7:45 AM UTC

@ABasi.2 wrote:

but why? 


Not everyone uses (or wants to use) CubeMX ?

It demonstrates that life without CubeMX is possible ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Jul 1, 2025 3:00 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.