Skip to main content
Associate II
Oct 15, 2024 7:45 AM UTC
Question

BLE extended advertising parsing

 

Hello Team ST,

I am currently working on parsing my extended BLE data using the BLE_p2pClient_Ext application, specifically the `analyse_ext_adv_report` function to view the advertising data. However, I am having trouble parsing and appending the full extended advertising data. Could you please assist me with this issue?

Thank you in advance.

Here is my modified function.

 

 

 

static uint8_t analyse_ext_adv_report(hci_le_extended_advertising_report_event_rp0 *p_ext_adv_report) {
 uint8_t status;
 
 if ((display_filter != 0) && HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0010)) {
 status = 1;
 } else {
 status = 0;
 
 l_buff_pos = 0;
 memset(&l_buff[l_buff_pos], 0, L_BUFF_SIZE);

 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, 
 "%02X:%02X:%02X:%02X:%02X:%02X | ", 
 p_ext_adv_report->Address[5], p_ext_adv_report->Address[4],
 p_ext_adv_report->Address[3], p_ext_adv_report->Address[2],
 p_ext_adv_report->Address[1], p_ext_adv_report->Address[0]);

 // Check for legacy or extended advertisement
 if (HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0010)) {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE, "LEGACY |");
 } else {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE, "EXTENDED |");
 }

 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "%4d | ", (int8_t)p_ext_adv_report->RSSI);
 
 // Connection and scanning status
 if (HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0001)) {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "CONN |");
 } else {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, " |");
 }

 if (HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0002)) {
 if (HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0008)) {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "SCAN RSP |");
 } else {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "SCAN |");
 }
 } else {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, " |");
 }

 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "%3d | ", p_ext_adv_report->Data_Length);

 if (p_ext_adv_report->Advertising_SID != 0xFF) {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "%2d | ", p_ext_adv_report->Advertising_SID);
 }

 if (HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0020)) {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "more data | ");
 } else if (HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0040)) {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "trunc data | ");
 } else {
 /* Nothing to do */
 }

 // Extended advertisement and non-connectable/non-scannable advertisements
 if (!(HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0010)) && // Extended
 !(HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0001)) && // Non-connectable
 !(HAL_IS_BIT_SET(p_ext_adv_report->Event_Type, 0x0002))) { // Non-scannable

 uint8_t i = 0, adtype, adlength;
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "ADV Data: ");

 // Loop through the entire advertising data
 while (i < p_ext_adv_report->Data_Length) {
 adlength = p_ext_adv_report->Data[i];
 adtype = p_ext_adv_report->Data[i + 1];

 // Print each chunk of advertising data in hex
 for (uint8_t j = 0; j < adlength + 1; j++) {
 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "%02X ", p_ext_adv_report->Data[i + j]);
 }
 i += adlength + 1;
 }
 }

 l_buff_pos += snprintf(&l_buff[l_buff_pos], L_BUFF_SIZE - l_buff_pos, "\n");

 // Debug output for the full advertising data
 APP_DBG_MSG("%s", l_buff);
 }
 
 return status;
}

 

 

 

 

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
Oct 15, 2024 10:07 AM UTC

Hello @Hardik02 

For more information about the Extended advertising on the STM32WB/WBA, you can check this wiki. 

You can also have a look at the implementation on these examples. It should help you to understand what to do.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Hardik02Author
Associate II
Oct 23, 2024 12:52 PM UTC

Hello,

I have gone through each example provided by you, but this can not solve my problem. 

regards