Skip to main content
Associate II
Dec 23, 2025 9:01 AM UTC
Solved

BLE disconnection problem on Android 15

I enabled the bonding feature in STM32WB5MMGH6TR.

abhi4_0-1766479530563.pngabhi4_1-1766479549092.png

Bonding is working correctly. But when the device(STM32WB) is bonded to phone(Android 15), calling disconnect from the phone does not disconnect the device.

This problem does not occur when:-

1. Phone Android version is less than 15(even after bonding it can disconnect).

2. Device is not bonded to the phone(Android 15).

abhi4Best answer
Associate II
Jan 14, 2026 9:51 AM UTC

It appears that this is the behaviour in Android versions 15 and above. Now, we are calling disconnect from the STM32WB (peripheral) upon receiving a command from the phone.

hci_disconnect(Connection_Handle, 0x13); //called to disconnect

1 reply

abhi4AuthorBest answer
Associate II
Jan 14, 2026 9:51 AM UTC

It appears that this is the behaviour in Android versions 15 and above. Now, we are calling disconnect from the STM32WB (peripheral) upon receiving a command from the phone.

hci_disconnect(Connection_Handle, 0x13); //called to disconnect