Skip to main content
Visitor II
Sep 10, 2026 9:56 AM UTC
Question

BLE Data Throughput regression on NUCLEO-WBA65RI (Server) with STM32CubeWBA v1.8.0 vs v1.7.0

Hello,

I'm running the BLE_DataThroughput_Server Application on a NUCLEO-WBA65RI (server, notifying) connected to a NUCLEO-WBA55CG (client, receiving notifications), and I'm seeing a significant throughput regression between STM32CubeWBA v1.7.0 and upper versions, with strictly identical configuration.

 

Setup (identical in both cases):

  • Server: NUCLEO-WBA65RI, BLE_DataThroughput_Server Application, from STM32CubeWBA v1.7.0, v1.8.0, and v1.10.0
  • Client: NUCLEO-WBA55CG,  BLE_DataThroughput_Client Application, from STM32CubeWBA v1.10.0

  • Connection interval: 11.25 ms
  • PHY: 2M
  • MTU size : 244
  • Build configuration: Release
  • I added :

const uint8_t a_BLE_rx_pckt_count_and_rx_pckt_len[2] = { 0x07, 0x00 }; /* rx_pckt_count , rx_pckt_len */ aci_hal_write_config_data(CONFIG_DATA_LL_RX_ACL_CTRL_OFFSET, 2, a_BLE_rx_pckt_count_and_rx_pckt_len);

as described in the "How to get the best throughput" section of the wiki (rx_pckt_count=7, rx_pckt_len=0)

 

Results:

  • BLE_DataThroughput_Server Application from STM32CubeWBA v1.7.0 → ~130 KB/s (consistent with the ~120 KB/s figure in the throughput measurement wiki page)
  • BLE_DataThroughput_Server Application from STM32CubeWBA v1.8.0 and v1.10.0 → ~58 KB/s, same hardware, same config, no other code change

 

Questions:

I see in the v1.8.0 release note :

BLE:

  • Support of BLE 6.0
  • Man-In-The-Middle (MITM) management is enhanced in the BLE stack to provide more flexibility and better interoperability.
  • Add BLE Host Stack events FIFO buffer mechanism
  1. Is this a known regression from v1.8.0 ?
  2. Is there a fix planned, or a recommended workaround to recover v1.7.0 throughput level, while staying on v1.8.0 or upper versions ?

 

Happy to share full traces / project files if useful.

Thanks in advance.

1 reply

ST Technical Moderator
Sep 22, 2026 1:22 PM UTC

Hello,

I am not able to reproduce your issue on v1.10.

My setup:

  • 2x Nucleo WBA65
  • BLE_DT_Server / BLE_DT_Client based on v1.10

Without the DT optimization for notifications from server to client, I get 65 KB/s.
With the optimization, I get 130 KB/s.

Are you still reproducing the issue since you reported it?
If so, would it be possible for you to capture an over-the-air trace with a BLE sniffer ?
 

Best regards,
Joé