Skip to main content
Yusuf
Associate II
Jul 14, 2023 11:41 AM UTC
Solved

BLE Advertising Problem

Hello,

I am working on a STM32WB55RG BLE Project and the problem is that about once in every 3 program that I upload, BLE doesn't work. After reupdating the BLE Stack firmware, it works correctly. I am using the BLE firmware v1.16.0.4.  What could be the problem?

 

Best Regards,

Yusuf

This topic has been closed for replies.
Yusuf
YusufBest answer
Associate II
Jul 21, 2023 1:37 PM UTC

Hello, I used STM32-USB-VCOM example shared by STM on custom board. However, I seen the same problem using P-Nucleo-WB55 dongle with Heart Rate example. I used the fix you have shared in Solved: STOP2 low power on STM32WB55 with BLE connection w... - STMicroelectronics Community  and now it seems fixed for now but I will continue to check it.

Best Regards,

2 replies

Remy ISSALYS
ST Technical Moderator
Jul 20, 2023 4:28 PM UTC

Hello,

Can you give more details on your issue? Are you using application form STM32CubeWB package or you have create your application ? Are you working on nucleo board or on custome hardware ?

Best Regards

Yusuf
YusufAuthorBest answer
Associate II
Jul 21, 2023 1:37 PM UTC

Hello, I used STM32-USB-VCOM example shared by STM on custom board. However, I seen the same problem using P-Nucleo-WB55 dongle with Heart Rate example. I used the fix you have shared in Solved: STOP2 low power on STM32WB55 with BLE connection w... - STMicroelectronics Community  and now it seems fixed for now but I will continue to check it.

Best Regards,