Skip to main content
asala.19
Associate III
Apr 20, 2020 10:29 AM UTC
Solved

Bin file size is too large

Hi,

I want to generate .bin file of BLE_OTA example.

i have added below command in post-build steps AC6 IDE.

arm-none-eabi-objcopy -O binary "${BuildArtifactFileBaseName}.elf" "${BuildArtifactFileBaseName}.bin"

It generate binary successfully but it's size is too larger than .elf and .hex, Please help me to resolve the above issue

Files size

Production.bin 385M

Production.hex 43K

Production.elf 2.0M

Thanks,

Arjun

This topic has been closed for replies.
asala.19
asala.19Best answer
Associate III
Apr 21, 2020 8:13 AM UTC

Hi ,

Thanks for your support i resolve above issue by changing below line in linker file

-- MB_MEM2 : { *(MB_MEM2) } >RAM_SHARED

++MB_MEM2 (NOLOAD) : { *(MB_MEM2) } >RAM_SHARED

Thanks,

Arjun

3 replies

Uwe Bonnes
Chief
Apr 20, 2020 10:44 AM UTC

Your bin file contains either data for RAM or external flash. Those are places at 0x2000000 or above and far awau from fl;ash at 0x800000. Bin files have no mean to indicate empty space, so they pad.

Review your linker file.

asala.19
asala.19Author
Associate III
Apr 20, 2020 10:57 AM UTC

Hi,

Thanks for quick response i use default linker file available with example code please tell what should i change in below linker file

/* Entry Point */
ENTRY(Reset_Handler)
 
/* Highest address of the user mode stack */
_estack = 0x20030000; /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x400; /* required amount of heap */
_Min_Stack_Size = 0x1000; /* required amount of stack */
 
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 512K
RAM1 (xrw) : ORIGIN = 0x20000004, LENGTH = 0x2FFFC
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10K
}
 
/* Define output sections */
SECTIONS
{
 /* The startup code goes first into FLASH */
 .isr_vector :
 {
 . = ALIGN(4);
 KEEP(*(.isr_vector)) /* Startup code */
 . = ALIGN(4);
 } >FLASH
 
 /* The program code and other data goes into FLASH */
 .text :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 *(.glue_7) /* glue arm to thumb code */
 *(.glue_7t) /* glue thumb to arm code */
 *(.eh_frame)
 
 KEEP (*(.init))
 KEEP (*(.fini))
 
 . = ALIGN(4);
 _etext = .; /* define a global symbols at end of code */
 } >FLASH
 
 /* Constant data goes into FLASH */
 .rodata :
 {
 . = ALIGN(4);
 *(.rodata) /* .rodata sections (constants, strings, etc.) */
 *(.rodata*) /* .rodata* sections (constants, strings, etc.) */
 . = ALIGN(4);
 } >FLASH
 
 .ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >FLASH
 .ARM : {
 __exidx_start = .;
 *(.ARM.exidx*)
 __exidx_end = .;
 } >FLASH
 
 .preinit_array :
 {
 PROVIDE_HIDDEN (__preinit_array_start = .);
 KEEP (*(.preinit_array*))
 PROVIDE_HIDDEN (__preinit_array_end = .);
 } >FLASH
 .init_array :
 {
 PROVIDE_HIDDEN (__init_array_start = .);
 KEEP (*(SORT(.init_array.*)))
 KEEP (*(.init_array*))
 PROVIDE_HIDDEN (__init_array_end = .);
 } >FLASH
 .fini_array :
 {
 PROVIDE_HIDDEN (__fini_array_start = .);
 KEEP (*(SORT(.fini_array.*)))
 KEEP (*(.fini_array*))
 PROVIDE_HIDDEN (__fini_array_end = .);
 } >FLASH
 
 /* used by the startup to initialize data */
 _sidata = LOADADDR(.data);
 
 /* Initialized data sections goes into RAM, load LMA copy after code */
 .data : 
 {
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.data) /* .data sections */
 *(.data*) /* .data* sections */
 
 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */
 } >RAM1 AT> FLASH
 
 
 /* Uninitialized data section */
 . = ALIGN(4);
 .bss :
 {
 /* This is used by the startup in order to initialize the .bss secion */
 _sbss = .; /* define a global symbol at bss start */
 __bss_start__ = _sbss;
 *(.bss)
 *(.bss*)
 *(COMMON)
 
 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
 } >RAM1
 
 /* User_heap_stack section, used to check that there is enough RAM left */
 ._user_heap_stack :
 {
 . = ALIGN(8);
 PROVIDE ( end = . );
 PROVIDE ( _end = . );
 . = . + _Min_Heap_Size;
 . = . + _Min_Stack_Size;
 . = ALIGN(8);
 } >RAM1
 
 
 
 /* Remove information from the standard libraries */
 /DISCARD/ :
 {
 libc.a ( * )
 libm.a ( * )
 libgcc.a ( * )
 }
 
 .ARM.attributes 0 : { *(.ARM.attributes) }
 MAPPING_TABLE (NOLOAD) : { *(MAPPING_TABLE) } >RAM_SHARED
 MB_MEM1 (NOLOAD) : { *(MB_MEM1) } >RAM_SHARED
 MB_MEM2 : { *(MB_MEM2) } >RAM_SHARED 
}

Thanks,

Arjun

asala.19
asala.19AuthorBest answer
Associate III
Apr 21, 2020 8:13 AM UTC

Hi ,

Thanks for your support i resolve above issue by changing below line in linker file

-- MB_MEM2 : { *(MB_MEM2) } >RAM_SHARED

++MB_MEM2 (NOLOAD) : { *(MB_MEM2) } >RAM_SHARED

Thanks,

Arjun