Battery percentage level varying often for each uplink when b-l072z-lrwan1 board powered with batteries.
Running " i-cube-lrwan - End node" firmware on board. We are expecting consistent battery percentage but observing inconsistent in battery percentage.
e.g. At first when battery is fully charged, it should show 100%. Later on as battery started draining percentage should decrease linearly.
But we are observing non linear change in battery percentage. Like
- 87%
- 87%
- 95%
- 80%
- 100%
We observed that +Vref voltage itself is fluctuating for each uplink when powered with batteries. So we are suspecting variation in Vref might be the reason. If so how to resolve this issue or is there any other reason for this??