B-WL5M-SUBG1 LoRaWAN_End_Node Application Time Delay For Tx Operation
- 4 replies
- 761 views
Hi,
I have a B-WL5M-SUBG1 board and I built ST's official LoRaWAN_End_Node application that I got from github and deployed to the board successfully. I changed the activation type as ABP (Activation By Personalization) and observed the logs via serial port. Tx operation happens in every 10 sec. for a while then the log says for example "4378s018:Next Tx in : ~2871 second(s)" and stops, after something close to 2871 sec. it starts Tx operation again. It keeps going like this in a stable way.
Some Tx operation - stops for 2871 sec. - some Tx operation again - stops for 2871 sec. - .................
I tracked this line in the source code a bit but I couldn't find the place I need to adjust in order to change this time limit or remove it totally. Furthermore why there is such a process?
By the way, in the sys_conf.h file it is configured like this "#define LOW_POWER_DISABLE 0", means low power mode is enabled.
Any help will be appreciated.
Here is some log as an example:
[INFO] Connected to STMicroelectronics STLink Virtual COM Port (COM7) at 115200 baud.
[2025-05-28 15:23:06] 0s427:APPLICATION STARTED
[2025-05-28 15:23:06] 0s427:LoRaWAN_Class: CLASS_A
[2025-05-28 15:23:06] 0s427:TX_Power: 0
[2025-05-28 15:23:06] 0s427:Activation_Type: ABP
[2025-05-28 15:23:06] 0s427:Tx_Periodicity: 10000 ms | 10 second
[2025-05-28 15:23:06] APPLICATION_VERSION: V1.3.1
[2025-05-28 15:23:06] MW_LORAWAN_VERSION: V2.6.1
[2025-05-28 15:23:06] MW_RADIO_VERSION: V1.3.1
[2025-05-28 15:23:06] L2_SPEC_VERSION: V1.0.4
[2025-05-28 15:23:06] RP_SPEC_VERSION: V2-1.0.3
[2025-05-28 15:23:35] 29s993:VDDA: 254
[2025-05-28 15:23:35] 29s993:temp: 18
[2025-05-28 15:23:35] 29s993:Sending the payload: Hello ST Community
[2025-05-28 15:23:35] 30s000:TX on freq 868300000 Hz at DR 0
[2025-05-28 15:23:35] 30s001:SEND REQUEST
[2025-05-28 15:23:37] 31s813:MAC txDone
[2025-05-28 15:23:38] 32s845:RX_1 on freq 868300000 Hz at DR 0
[2025-05-28 15:23:38] 33s043:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:23:38] 33s043:MAC rxTimeOut
[2025-05-28 15:23:39] 33s845:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:23:39] 34s043:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:23:39] 34s043:MAC rxTimeOut
[2025-05-28 15:23:39]
[2025-05-28 15:23:39] ###### ========== MCPS-Confirm =============
[2025-05-28 15:23:39] ###### U/L FRAME:0001 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:24:05] 59s536:VDDA: 254
[2025-05-28 15:24:05] 59s536:temp: 18
[2025-05-28 15:24:05] 59s536:Sending the payload: Hello ST Community
[2025-05-28 15:24:05] 59s540:TX on freq 868300000 Hz at DR 0
[2025-05-28 15:24:05] 59s542:SEND REQUEST
[2025-05-28 15:24:07] 61s353:MAC txDone
[2025-05-28 15:24:08] 62s385:RX_1 on freq 868300000 Hz at DR 0
[2025-05-28 15:24:08] 62s583:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:24:08] 62s583:MAC rxTimeOut
[2025-05-28 15:24:09] 63s385:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:24:09] 63s583:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:24:09] 63s583:MAC rxTimeOut
[2025-05-28 15:24:09]
[2025-05-28 15:24:09] ###### ========== MCPS-Confirm =============
[2025-05-28 15:24:09] ###### U/L FRAME:0002 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:24:34] 89s076:VDDA: 254
[2025-05-28 15:24:34] 89s076:temp: 18
[2025-05-28 15:24:34] 89s076:Sending the payload: Hello ST Community
[2025-05-28 15:24:34] 89s080:TX on freq 868300000 Hz at DR 0
[2025-05-28 15:24:34] 89s082:SEND REQUEST
[2025-05-28 15:24:36] 90s893:MAC txDone
[2025-05-28 15:24:37] 91s925:RX_1 on freq 868300000 Hz at DR 0
[2025-05-28 15:24:37] 92s124:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:24:37] 92s124:MAC rxTimeOut
[2025-05-28 15:24:38] 92s925:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:24:38] 93s124:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:24:38] 93s124:MAC rxTimeOut
[2025-05-28 15:24:38]
[2025-05-28 15:24:38] ###### ========== MCPS-Confirm =============
[2025-05-28 15:24:38] ###### U/L FRAME:0003 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:25:04] 118s616:VDDA: 254
[2025-05-28 15:25:04] 118s616:temp: 18
[2025-05-28 15:25:04] 118s616:Sending the payload: Hello ST Community
[2025-05-28 15:25:04] 118s620:TX on freq 868300000 Hz at DR 0
[2025-05-28 15:25:04] 118s622:SEND REQUEST
[2025-05-28 15:25:06] 120s432:MAC txDone
[2025-05-28 15:25:07] 121s464:RX_1 on freq 868300000 Hz at DR
[2025-05-28 15:25:07] 121s663:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:25:07] 121s663:MAC rxTimeOut
[2025-05-28 15:25:08] 122s464:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:25:08] 122s663:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:25:08] 122s663:MAC rxTimeOut
[2025-05-28 15:25:08]
[2025-05-28 15:25:08] ###### ========== MCPS-Confirm =============
[2025-05-28 15:25:08] ###### U/L FRAME:0004 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:25:33] 148s156:VDDA: 254
[2025-05-28 15:25:33] 148s156:temp: 18
[2025-05-28 15:25:33] 148s156:Sending the payload: Hello ST Community
[2025-05-28 15:25:33] 148s160:TX on freq 868500000 Hz at DR 0
[2025-05-28 15:25:33] 148s163:SEND REQUEST
[2025-05-28 15:25:35] 149s973:MAC txDone
[2025-05-28 15:25:36] 151s005:RX_1 on freq 868500000 Hz at DR 0
[2025-05-28 15:25:36] 151s204:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:25:36] 151s204:MAC rxTimeOut
[2025-05-28 15:25:37] 152s005:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:25:37] 152s204:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:25:37] 152s204:MAC rxTimeOut
[2025-05-28 15:25:37]
[2025-05-28 15:25:37] ###### ========== MCPS-Confirm =============
[2025-05-28 15:25:37] ###### U/L FRAME:0005 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:26:03] 177s696:VDDA: 254
[2025-05-28 15:26:03] 177s696:temp: 18
[2025-05-28 15:26:03] 177s696:Sending the payload: Hello ST Community
[2025-05-28 15:26:03] 177s700:TX on freq 868500000 Hz at DR 0
[2025-05-28 15:26:03] 177s703:SEND REQUEST
[2025-05-28 15:26:05] 179s513:MAC txDone
[2025-05-28 15:26:06] 180s545:RX_1 on freq 868500000 Hz at DR 0
[2025-05-28 15:26:06] 180s744:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:26:06] 180s744:MAC rxTimeOut
[2025-05-28 15:26:07] 181s545:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:26:07] 181s744:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:26:07] 181s744:MAC rxTimeOut
[2025-05-28 15:26:07]
[2025-05-28 15:26:07] ###### ========== MCPS-Confirm =============
[2025-05-28 15:26:07] ###### U/L FRAME:0006 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:26:32] 207s236:VDDA: 254
[2025-05-28 15:26:32] 207s236:temp: 18
[2025-05-28 15:26:32] 207s236:Sending the payload: Hello ST Community
[2025-05-28 15:26:32] 207s240:TX on freq 868500000 Hz at DR 0
[2025-05-28 15:26:32] 207s243:SEND REQUEST
[2025-05-28 15:26:34] 209s053:MAC txDone
[2025-05-28 15:26:35] 210s085:RX_1 on freq 868500000 Hz at DR
[2025-05-28 15:26:35] 210s284:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:26:35] 210s284:MAC rxTimeOut
[2025-05-28 15:26:36] 211s085:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:26:36] 211s284:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:26:36] 211s284:MAC rxTimeOut
[2025-05-28 15:26:36]
[2025-05-28 15:26:36] ###### ========== MCPS-Confirm =============
[2025-05-28 15:26:36] ###### U/L FRAME:0007 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:27:02] 236s776:VDDA: 254
[2025-05-28 15:27:02] 236s776:temp: 18
[2025-05-28 15:27:02] 236s776:Sending the payload: Hello ST Community
[2025-05-28 15:27:02] 236s780:TX on freq 868100000 Hz at DR 0
[2025-05-28 15:27:02] 236s783:SEND REQUEST
[2025-05-28 15:27:04] 238s593:MAC txDone
[2025-05-28 15:27:05] 239s625:RX_1 on freq 868100000 Hz at DR 0
[2025-05-28 15:27:05] 239s824:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:27:05] 239s824:MAC rxTimeOut
[2025-05-28 15:27:06] 240s625:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:27:06] 240s824:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:27:06] 240s824:MAC rxTimeOut
[2025-05-28 15:27:06]
[2025-05-28 15:27:06] ###### ========== MCPS-Confirm =============
[2025-05-28 15:27:06] ###### U/L FRAME:0008 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:27:31] 266s316:VDDA: 254
[2025-05-28 15:27:31] 266s316:temp: 18
[2025-05-28 15:27:32] 266s316:Sending the payload: Hello ST Community
[2025-05-28 15:27:32] 266s320:TX on freq 868300000 Hz at DR 0
[2025-05-28 15:27:32] 266s323:SEND REQUEST
[2025-05-28 15:27:33] 268s133:MAC txDone
[2025-05-28 15:27:34] 269s166:RX_1 on freq 868300000 Hz at DR 0
[2025-05-28 15:27:35] 269s364:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:27:35] 269s364:MAC rxTimeOut
[2025-05-28 15:27:35] 270s166:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:27:36] 270s364:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:27:36] 270s364:MAC rxTimeOut
[2025-05-28 15:27:36]
[2025-05-28 15:27:36] ###### ========== MCPS-Confirm =============
[2025-05-28 15:27:36] ###### U/L FRAME:0009 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:28:01] 295s856:VDDA: 254
[2025-05-28 15:28:01] 295s856:temp: 18
[2025-05-28 15:28:01] 295s856:Sending the payload: Hello ST Community
[2025-05-28 15:28:01] 295s860:TX on freq 868500000 Hz at DR 0
[2025-05-28 15:28:01] 295s863:SEND REQUEST
[2025-05-28 15:28:03] 297s673:MAC txDone
[2025-05-28 15:28:04] 298s706:RX_1 on freq 868500000 Hz at DR 0
[2025-05-28 15:28:04] 298s904:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:28:04] 298s904:MAC rxTimeOut
[2025-05-28 15:28:05] 299s706:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:28:05] 299s904:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:28:05] 299s904:MAC rxTimeOut
[2025-05-28 15:28:05]
[2025-05-28 15:28:05] ###### ========== MCPS-Confirm =============
[2025-05-28 15:28:05] ###### U/L FRAME:0010 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:28:31] 325s396:VDDA: 254
[2025-05-28 15:28:31] 325s396:temp: 18
[2025-05-28 15:28:31] 325s396:Sending the payload: Hello ST Community
[2025-05-28 15:28:31] 325s400:TX on freq 868500000 Hz at DR 0
[2025-05-28 15:28:31] 325s403:SEND REQUEST
[2025-05-28 15:28:32] 327s213:MAC txDone
[2025-05-28 15:28:33] 328s246:RX_1 on freq 868500000 Hz at DR 0
[2025-05-28 15:28:34] 328s444:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:28:34] 328s444:MAC rxTimeOut
[2025-05-28 15:28:34] 329s246:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:28:35] 329s444:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:28:35] 329s444:MAC rxTimeOut
[2025-05-28 15:28:35]
[2025-05-28 15:28:35] ###### ========== MCPS-Confirm =============
[2025-05-28 15:28:35] ###### U/L FRAME:0011 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:29:00] 354s936:VDDA: 254
[2025-05-28 15:29:00] 354s936:temp: 18
[2025-05-28 15:29:00] 354s936:Sending the payload: Hello ST Communit
[2025-05-28 15:29:00] 354s940:TX on freq 868500000 Hz at DR 0
[2025-05-28 15:29:00] 354s943:SEND REQUEST
[2025-05-28 15:29:02] 356s753:MAC txDone
[2025-05-28 15:29:03] 357s786:RX_1 on freq 868500000 Hz at DR 0
[2025-05-28 15:29:03] 357s984:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:29:03] 357s984:MAC rxTimeOut
[2025-05-28 15:29:04] 358s786:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:29:04] 358s984:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:29:04] 358s984:MAC rxTimeOut
[2025-05-28 15:29:04]
[2025-05-28 15:29:04] ###### ========== MCPS-Confirm =============
[2025-05-28 15:29:04] ###### U/L FRAME:0012 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:29:30] 384s476:VDDA: 254
[2025-05-28 15:29:30] 384s476:temp: 18
[2025-05-28 15:29:30] 384s476:Sending the payload: Hello ST Community
[2025-05-28 15:29:30] 384s480:TX on freq 868100000 Hz at DR 0
[2025-05-28 15:29:30] 384s483:SEND REQUEST
[2025-05-28 15:29:31] 386s293:MAC txDone
[2025-05-28 15:29:32] 387s326:RX_1 on freq 868100000 Hz at DR 0
[2025-05-28 15:29:33] 387s524:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:29:33] 387s524:MAC rxTimeOut
[2025-05-28 15:29:33] 388s326:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:29:34] 388s524:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:29:34] 388s524:MAC rxTimeOut
[2025-05-28 15:29:34
[2025-05-28 15:29:34] ###### ========== MCPS-Confirm =============
[2025-05-28 15:29:34] ###### U/L FRE:0013 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:29:59] 414s016:VDDA: 25
[2025-05-28 15:29:59] 414s016:temp: 18
[2025-05-28 15:29:59] 414s016:Sending the payload: Hello ST Community
[2025-05-28 15:29:59] 414s020:TX on freq 868500000 Hz at DR 0
[2025-05-28 15:29:59] 414s023:SEND REQUEST
[2025-05-28 15:30:01] 415s833:MAC txDone
[2025-05-28 15:30:02] 416s866:RX_1 on freq 868500000 Hz at DR 0
[2025-05-28 15:30:02] 417s064:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:30:02] 417s064:MAC rxTimeOut
[2025-05-28 15:30:03] 417s866:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:30:03] 418s064:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:30:03] 418s064:MAC rxTimeOut
[2025-05-28 15:30:03]
[2025-05-28 15:30:03] ###### ========== MCPS-Confirm =============
[2025-05-28 15:30:03] ###### U/L FRAME:0014 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:30:29] 443s556:VDDA: 254
[2025-05-28 15:30:29] 443s556:temp: 18
[2025-05-28 15:30:29] 443s556:Sending the payload: Hello ST Community
[2025-05-28 15:30:29] 443s560:TX on freq 868500000 Hz at DR 0
[2025-05-28 15:30:29] 443s563:SEND REQUEST
[2025-05-28 15:30:31] 445s374:MAC txDone
[2025-05-28 15:30:32] 446s407:RX_1 on freq 868500000 Hz at DR 0
[2025-05-28 15:30:32] 446s605:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:30:32] 446s605:MAC rxTimeOut
[2025-05-28 15:30:33] 447s407:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:30:33] 447s605:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:30:33] 447s605:MAC rxTimeOut
[2025-05-28 15:30:33]
[2025-05-28 15:30:33] ###### ========== MCPS-Confirm =============
[2025-05-28 15:30:33] ###### U/L FRAME:0015 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:30:58] 473s096:VDDA: 254
[2025-05-28 15:30:58] 473s096:temp: 18
[2025-05-28 15:30:58] 473s096:Sending the payload: Hello ST Community
[2025-05-28 15:30:58] 473s100:TX on freq 868300000 Hz at DR 0
[2025-05-28 15:30:58] 473s103:SEND REQUEST
[2025-05-28 15:31:00] 474s914:MAC txDone
[2025-05-28 15:31:01] 475s946:RX_1 on freq 868300000 Hz at DR 0
[2025-05-28 15:31:01] 476s144:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:31:01] 476s144:MAC rxTimeOut
[2025-05-28 15:31:02] 476s946:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:31:02] 477s144:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:31:02] 477s144:MAC rxTimeOut
[2025-05-28 15:31:02]
[2025-05-28 15:31:02] ###### ========== MCPS-Confirm =============
[2025-05-28 15:31:02] ###### U/L FRAME:0016 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:31:28] 502s636:VDDA: 254
[2025-05-28 15:31:28] 502s636:temp: 18
[2025-05-28 15:31:28] 502s636:Sending the payload: Hello ST Community
[2025-05-28 15:31:28] 502s640:TX on freq 868300000 Hz at DR 0
[2025-05-28 15:31:28] 502s643:SEND REQUEST
[2025-05-28 15:31:30] 504s454:MAC txDone
[2025-05-28 15:31:31] 505s486:RX_1 on freq 868300000 Hz at DR 0
[2025-05-28 15:31:31] 505s684:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:31:31] 505s684:MAC rxTimeOut
[2025-05-28 15:31:32] 506s486:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:31:32] 506s684:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:31:32] 506s684:MAC rxTimeOut
[2025-05-28 15:31:32]
[2025-05-28 15:31:32] ###### ========== MCPS-Confirm =============
[2025-05-28 15:31:32] ###### U/L FRAME:0017 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:31:57] 532s176:VDDA: 254
[2025-05-28 15:31:57] 532s176:temp: 18
[2025-05-28 15:31:57] 532s176:Sending the payload: Hello ST Community
[2025-05-28 15:31:57] 532s180:TX on freq 868100000 Hz at DR 0
[2025-05-28 15:31:57] 532s183:SEND REQUEST
[2025-05-28 15:31:59] 533s994:MAC txDone
[2025-05-28 15:32:00] 535s026:RX_1 on freq 868100000 Hz at DR 0
[2025-05-28 15:32:00] 535s224:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:32:00] 535s224:MAC rxTimeOut
[2025-05-28 15:32:01] 536s026:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:32:01] 536s224:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:32:01] 536s224:MAC rxTimeOut
[2025-05-28 15:32:01]
[2025-05-28 15:32:01] ###### ========== MCPS-Confirm =============
[2025-05-28 15:32:01] ###### U/L FRAME:0018 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:32:27] 561s716:VDDA: 254
[2025-05-28 15:32:27] 561s716:temp: 18
[2025-05-28 15:32:27] 561s716:Sending the payload: Hello ST Community
[2025-05-28 15:32:27] 561s720:TX on freq 868300000 Hz at DR 0
[2025-05-28 15:32:27] 561s723:SEND REQUEST
[2025-05-28 15:32:29] 563s534:MAC txDone
[2025-05-28 15:32:30] 564s566:RX_1 on freq 868300000 Hz at DR 0
[2025-05-28 15:32:30] 564s764:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:32:30] 564s764:MAC rxTimeOut
[2025-05-28 15:32:31] 565s566:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 15:32:31] 565s764:IRQ_RX_TX_TIMEOUT
[2025-05-28 15:32:31] 565s764:MAC rxTimeOut
[2025-05-28 15:32:31]
[2025-05-28 15:32:31] ###### ========== MCPS-Confirm =============
[2025-05-28 15:32:31] ###### U/L FRAME:0019 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 15:32:56] 591s256:VDDA: 254
[2025-05-28 15:32:56] 591s256:temp: 18
[2025-05-28 15:32:56] 591s256:Sending the payload: Hello ST Community
[2025-05-28 15:32:56] 591s256:Next Tx in : ~3038 second(s)
[2025-05-28 15:33:16] 610s790:VDDA: 254
[2025-05-28 15:33:16] 610s790:temp: 18
[2025-05-28 15:33:16] 610s790:Sending the payload: Hello ST Community
[2025-05-28 15:33:16] 610s790:Next Tx in : ~3019 second(s)
[2025-05-28 16:23:54] 3649s525:VDDA: 254
[2025-05-28 16:23:54] 3649s525:temp: 18
[2025-05-28 16:23:54] 3649s525:Sending the payload: Hello ST Community
[2025-05-28 16:23:54] 3649s529:TX on freq 868100000 Hz at DR 0
[2025-05-28 16:23:54] 3649s532:SEND REQUEST
[2025-05-28 16:23:56] 3651s342:MAC txDone
[2025-05-28 16:23:57] 3652s375:RX_1 on freq 868100000 Hz at DR 0
[2025-05-28 16:23:57] 3652s573:IRQ_RX_TX_TIMEOUT
[2025-05-28 16:23:57] 3652s573:MAC rxTimeOut
[2025-05-28 16:23:58] 3653s375:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 16:23:58] 3653s573:IRQ_RX_TX_TIMEOUT
[2025-05-28 16:23:58] 3653s573:MAC rxTimeOut
[2025-05-28 16:23:58]
[2025-05-28 16:23:58] ###### ========== MCPS-Confirm =============
[2025-05-28 16:23:58] ###### U/L FRAME:0020 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 16:24:24] 3679s065:VDDA: 254
[2025-05-28 16:24:24] 3679s065:temp: 18
[2025-05-28 16:24:24] 3679s065:Sending the payload: Hello ST Community
[2025-05-28 16:24:24] 3679s069:TX on freq 868100000 Hz at DR 0
[2025-05-28 16:24:24] 3679s071:SEND REQUEST
[2025-05-28 16:24:26] 3680s882:MAC txDone
[2025-05-28 16:24:27] 3681s915:RX_1 on freq 868100000 Hz at DR 0
[2025-05-28 16:24:27] 3682s113:IRQ_RX_TX_TIMEOUT
[2025-05-28 16:24:27] 3682s113:MAC rxTimeOut
[2025-05-28 16:24:28] 3682s915:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 16:24:28] 3683s113:IRQ_RX_TX_TIMEOUT
[2025-05-28 16:24:28] 3683s113:MAC rxTimeOut
[2025-05-28 16:24:28]
[2025-05-28 16:24:28] ###### ========== MCPS-Confirm =============
[2025-05-28 16:24:28] ###### U/L FRAME:0021 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 16:24:53] 3708s605:VDDA: 254
[2025-05-28 16:24:53] 3708s605:temp: 18
[2025-05-28 16:24:53] 3708s605:Sending the payload: Hello ST Community
[2025-05-28 16:24:53] 3708s609:TX on freq 868300000 Hz at DR 0
[2025-05-28 16:24:53] 3708s612:SEND REQUEST
[2025-05-28 16:24:55] 3710s422:MAC txDone
[2025-05-28 16:24:56] 3711s455:RX_1 on freq 868300000 Hz at DR 0
[2025-05-28 16:24:56] 3711s653:IRQ_RX_TX_TIMEOUT
[2025-05-28 16:24:56] 3711s653:MAC rxTimeOut
[2025-05-28 16:24:57] 3712s455:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 16:24:57] 3712s653:IRQ_RX_TX_TIMEOUT
[2025-05-28 16:24:57] 3712s653:MAC rxTimeOut
*
*
*
*
*
[2025-05-28 16:32:20] ###### ========== MCPS-Confirm =============
[2025-05-28 16:32:20] ###### U/L FRAME:0037 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 16:32:46] 4181s246:VDDA: 254
[2025-05-28 16:32:46] 4181s246:temp: 18
[2025-05-28 16:32:46] 4181s246:Sending the payload: Hello ST Community
[2025-05-28 16:32:46] 4181s250:TX on freq 868500000 Hz at DR 0
[2025-05-28 16:32:46] 4181s252:SEND REQUEST
[2025-05-28 16:32:48] 4183s063:MAC txDone
[2025-05-28 16:32:49] 4184s095:RX_1 on freq 868500000 Hz at DR 0
[2025-05-28 16:32:49] 4184s293:IRQ_RX_TX_TIMEOUT
[2025-05-28 16:32:49] 4184s293:MAC rxTimeOut
[2025-05-28 16:32:50] 4185s095:RX_2 on freq 869525000 Hz at DR 0
[2025-05-28 16:32:50] 4185s293:IRQ_RX_TX_TIMEOUT
[2025-05-28 16:32:50] 4185s293:MAC rxTimeOut
[2025-05-28 16:32:50]
[2025-05-28 16:32:50] ###### ========== MCPS-Confirm =============
[2025-05-28 16:32:50] ###### U/L FRAME:0038 | PORT:2 | DR:0 | PWR:0 | MSG TYPE:UNCONFIRMED
[2025-05-28 16:33:15] 4210s786:VDDA: 254
[2025-05-28 16:33:15] 4210s786:temp: 18
[2025-05-28 16:33:15] 4210s786:Sending the payload: Hello ST Community
[2025-05-28 16:33:15] 4210s786:Next Tx in : ~3038 second(s)
[2025-05-28 16:33:35] 4230s319:VDDA: 254
[2025-05-28 16:33:35] 4230s319:temp: 18
[2025-05-28 16:33:35] 4230s319:Sending the payload: Hello ST Community
[2025-05-28 16:33:35] 4230s319:Next Tx in : ~3019 second(s)