Question
B-L072Z-LRWAN1 LoRa define EUIs
Posted on June 21, 2018 at 11:22
Hello,
I'm new to LoRa network, and I would like to use the B-L072Z-LRWAN1 board to exchange data with a server. I use the I-CUBE-LRWAN 'Ping Pong' project as a starting point. I'd like to modify the ping pong app to exchange data with the server, but I need to specify EUIs (App EUI, Dev EUI...) but I havent find where I can do that.
I have check this video, where EUIs are defined in Comissioning.h, but it is based on a P-NUCLEO-LRWAN1 kit :
Thanks !
Best Regards
Thomas
#b-l072z-lrwan1-lora-eui