Skip to main content
Associate III
Mar 27, 2026 8:38 AM UTC
Question

Auracast Receiver using using STM32WBA55G-DK1

Hi, 

I am using STM32WBA55G-DK1 as a BLE TMAP Peripheral, I have a transmitter, which is transmitting 4 channels/subgroups of data. But the device is stucking at Syncing PA, but when the same is given with 2 channels(BIS), I am able to to connect and listen the music. What are the changes to be made to avoid this issue.

 

Thank you

4 replies

ST Technical Moderator
Mar 29, 2026 3:53 PM UTC

Hello @Sandeep_k ,

First, check your STM32CubeWBA version; ensure that it supports more than 2 BIS (if it is older than V1.8.0, the maximum supported BIS is 2).

Bluetooth® Low Energy audio - STM32WBA Frequently Asked Question - stm32mcu

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Sandeep_kAuthor
Associate III
Mar 30, 2026 6:47 AM UTC

I am using STMCube IDE 2.0.0

ST Technical Moderator
Mar 30, 2026 7:54 AM UTC

I mean the version of the STM32Cube MCU Package for STM32WBA series: STM32CubeWBA.

(not the STM32CubeIDE development tool)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Apr 9, 2026 3:14 PM UTC

Hi @Sandeep_k ,

Did you solve this issue?

We would appreciate it if you could provide an update on this topic and confirm whether it has been resolved. This will help other Community users who have the same question.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks