Skip to main content
LDrey.1
Associate
Feb 14, 2023 10:40 AM UTC
Question

Applications uploaded to the Seeed Studio LoRa-E5 mini does not boot

My supervisor and I have been trying to do some work using the Seeed studio board LoRa-E5 mini using STM32WLE5JC.

After struggling a bit with removing the included write protection using the STM Programmer and a ST-Link, we managed to upload a script to the board. While we can, indeed see that the script has been uploaded, see picture attached below, the board seems to be entirely unresponsive. We can neither detect any activity on the connected serial ports, nor does the builtin LED flash (Code included below). We have also tried this on two boards, making it more unlikely to be caused by faulty hardware. The only response we have been able to get is that the RX LED flashes briefly if we send messages to it using the Arduino IDE (v2) serial monitor.

Has anyone encountered similar problems to ours?

Image showing that data has been uploaded to the controller: (We have also found machine instructions for writing to serial and blinking the built in LED in the system memory)

This topic has been closed for replies.

3 replies

LDrey.1
LDrey.1Author
Associate
Feb 14, 2023 10:40 AM UTC

The script we uploaded was a standard blink-script, namely

#include <Arduino.h>

void setup() {

// put your setup code here, to run once:

Serial.begin(115200);

delay(100);

Serial.println(F("booted"));

pinMode(LED_BUILTIN, OUTPUT); //We have tried using the exact pin name as well

digitalWrite(LED_BUILTIN, HIGH);

}

void loop() {

delay(2000);

Serial.println(F("loop"));

// put your main code here, to run repeatedly:

}

LDrey.1
LDrey.1Author
Associate
Mar 31, 2023 11:50 AM UTC

Found a solution to the issue. Instructions can be found here:

https://github.com/larswd/STM32WL-Seeed-LoRa-E5-mini-Playground

Visitor II
Feb 13, 2025 12:12 PM UTC

How did you remove the included write protection, when i connect the board (LoRa-E5-HF) to my PC it doesn't show up in device manager. What should i do?