Skip to main content
Associate II
August 21, 2026
Question

Android version for Drone remote controller app ST BLE Drone

  • August 21, 2026
  • 5 replies
  • 123 views

Hi,

I bought the STEVAL-DRONE02 and STEVALFCU001V2 last week. But I couldn’t download the Android app ST BLE Drone  on my smart phone which has Android version 14. 

Which Android version does ST_BLE_DRONE support?
I checked with Google and it say:

The ST BLE Drone application supports Android 4.4 and higher. It acts as a Bluetooth Low Energy (BLE) remote controller designed to work with evaluation boards like the STEVAL-FCU001V1.

5 replies

Karl Yamashita
Principal
August 21, 2026

I assume that Google Play does not give you an option to download to your current phone because it’s grayed out?

I’ve own several Google Pixel phones in the past and my current phone is a Pixel 10 Pro XL and none of those phones are supported. ST has not updated the app since March 2020. I wanted to return my drone kit which i bought directly from ST, but it’s like jumping through hoops to find a way to contact them to return it. So right now, it’s a paper weight.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
YCCAuthor
Associate II
August 21, 2026

Thanks for the info.

The Play Store on my phone doesn’t even show the ST BLE Drone app. Only when I search the app from Google, it says the app is not supported on my phone.

 

Karl Yamashita
Principal
August 21, 2026

Hopefully you have better luck in returning your kit for a refund.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
cartergray733
Explorer II
August 22, 2026

Android 14 should meet the stated Android 4.4+ requirement. The issue is likely that the ST BLE Drone app is outdated and no longer compatible with newer Android versions. Check ST’s latest software package or contact ST support for a newer APK/version.

YCCAuthor
Associate II
August 22, 2026

Thanks for the comments.

 

Just some update on the download and installation of the ST BLE Drone app.

After some Google search, I have managed to install the APK of the ST BLE Drone app to my tablet, which is running on Android 16, by following [1].  I found the app’s APK from online. Tablet is used instead of my smart phone because I don’t want to damage my phone if problem occur.

Now the ST app on my tablet is able to connect to the FCU, then calibrated and armed the FCU.

Anyway the Bluetooth remote connection step is completed.

 

Other notes:
1. I think I didn’t orientate the frame and motors/propeller correctly. 
2. On one of the motors, a wire is disconnected from motor. I may need to see how to attach the wire to the motor, or buy another set of motor.



Ref

[1] How To Allow Installation From Unknown Sources On Android (Samsung Galaxy) [YouTube]

[2] Getting Started with ST Mini Drone Kit [YouTube]