Skip to main content
MBeld.1
Associate
Sep 21, 2020 11:06 AM UTC
Solved

AN5129 antenna. Differences between application note and Nucleo implementation

Hi.

I'm wondering about discrepancies in antenna dimensions between AN5129 application note and the actual board - Nucleo MB1335. As you can see the differences are subtle but visible. I'm mostly curious about why the antenna width varies? Widths at different spots I was able to measure: 0.4mm, 0.425mm, 0.45mm, 0.475mm, 0.5mm.

Also, the gap between parallel arms varies between 0.725mm and 0.75mm, which is different than 0.8 specified in the app note.

Is there a reason for that or is it simply a mistake while doing a layout? I can see that the antenna wasn't defined as library component but rather drew as a polygon.

0693W000004GZNIQA4.png0693W000004GZQ2QAO.png

This topic has been closed for replies.
Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Sep 22, 2020 2:35 PM UTC

Just got the answer. In fact, this layout came from a previous design for which the antenna was fully validated for BLE communication. Some marginal adaptations were made after further tests on the first proto boards as it is hard to determine the exact parameters of the PCB.

Note that the width of the antenna has an impact on the impedance, radiation and bandwidth too. hence the differences you can see in between the theorical design in AN5129 and the effective design resulting from real tests.

6 replies

Remi QUINTIN
ST Technical Moderator
Sep 21, 2020 12:26 PM UTC

These variations results from the board manufacturing.

What is key is the length of the antenna which should be a multiple of the wavelength/4.

MBeld.1
MBeld.1Author
Associate
Sep 21, 2020 4:32 PM UTC

I didn't measure the actual board. The differences are on the design files, based on which the board is later manufactured.

Remi QUINTIN
ST Technical Moderator
Sep 21, 2020 7:34 PM UTC

​OK I understand. No idea for now. i will check with the board designer.

MBeld.1
MBeld.1Author
Associate
Sep 22, 2020 5:55 AM UTC

Thank you, appreciate it.

Remi QUINTIN
Remi QUINTINBest answer
ST Technical Moderator
Sep 22, 2020 2:35 PM UTC

Just got the answer. In fact, this layout came from a previous design for which the antenna was fully validated for BLE communication. Some marginal adaptations were made after further tests on the first proto boards as it is hard to determine the exact parameters of the PCB.

Note that the width of the antenna has an impact on the impedance, radiation and bandwidth too. hence the differences you can see in between the theorical design in AN5129 and the effective design resulting from real tests.

Remi QUINTIN
ST Technical Moderator
Sep 22, 2020 2:37 PM UTC

Note that the matching network is also a key element of the RF path to get an effective and performant antenna.