Question
ADC giving value of 4095 on all configured channel
- 4 replies
- 186 views
Hello Community,
I am working on a custom board using the STM32 MCU (STM32WLE5JCI6). I am configuring the ADC with two channels:
- PB1 → ADC_IN5
- PB3 → ADC_IN2
I performed the following test cases and observed unexpected ADC behavior.
Test Case 1
- Applied VDD+ to Channel 2 (ADC_IN2)
- Channel 5 (ADC_IN5) connected to GND
Observation:
Both ADC channels are reading 4095, even though Channel 5 is tied to GND.
Test Case 2
- Applied VDD+ to Channel 5 (ADC_IN5)
Observation:
Instead of getting 4095 on Channel 5, both channels are reading approximately 1500.
I am also facing the same issue with another MCU: STM32L071KBT6TR.
Development tools being used:
- STM32CubeIDE Version 2.1.0
- STM32CubeMX Version 6.8.0
I have attached the main source file containing the ADC configuration for reference.
Could anyone please help identify what might be causing this issue?
Awaiting your valuable suggestions.
Thanks.