Skip to main content
TomC
Senior
Jan 20, 2021 1:31 AM UTC
Solved

ADC: Cannot change channel.

Board: STM32WB55-NUCLEO Pack

I am unable to change the channel being read by the ADC using the included code.

I have set the number of conversion to 3 in the ADC configurations. I am not using the DMA but am polling.

uint32_t get_battery_voltage(){
 
	sConfig.Channel = ADC_CHANNEL_3 ;
	sConfig.Rank = 1;
	if (HAL_ADC_ConfigChannel(&hadc1,&sConfig) != HAL_OK)
	 {
	 Error_Handler();
	 }
 
	HAL_ADC_Start(&hadc1);
 
	if(HAL_ADC_PollForConversion(&hadc1,5)==HAL_OK){
	 state.battery_voltage = (double)(HAL_ADC_GetValue(&hadc1));	
	 state.battery_voltage = (state.battery_voltage/4095)*3.3;
	}
	HAL_Delay(50);
 
	HAL_ADC_Stop(&hadc1);
 
	return state.battery_voltage;
}

This topic has been closed for replies.
TomC
TomCBest answer
Senior
Jan 28, 2021 1:07 AM UTC

The reason I was unable to change channel correctly and thus read another ADC pin was because I did not specify the "Number of Conversions" as the number of channels I wished to use in the ADC's configuration.

6 replies

TDK
Jan 20, 2021 2:14 AM UTC

If you're converting multiple channels, they're probably overwriting each other and you're only reading the last one (i.e. rank 3) which is converted.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TomC
TomCAuthor
Senior
Jan 20, 2021 7:24 PM UTC

Hi TDK.

Are you saying that I'm not specifying which channel to read correctly so the program is only reading whatever's in rank 3? Why do you think that the program would only read rank 3 as opposed to 1 or 2?

Remi QUINTIN
ST Technical Moderator
Jan 20, 2021 4:47 PM UTC

>unable to change the channel being read by the ADC

What do you mean?

To read another channel, you have to set​ sConfig.Channel to another channel.

>I have set the number of conversion to 3 in the ADC configurations

Do you mean you want to perform 3 sucessive conversions?

Could you also show that configuration (hadc structure) in MX_ADC_Init function?

TomC
TomCAuthor
Senior
Jan 20, 2021 7:19 PM UTC

Hi Remi,

I mean that despite changing sConfig's channel, the data being generated by HAL_ADC_GetValue(&hadc1) is consistent with initial configuration set by MX_ADC1_Init(void). That is to say, I believe the channel specified by the sConfig object is not changing correctly. Please see the ADC initialization code:

/**
 * @brief ADC1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_ADC1_Init(void)
{
 
 /* USER CODE BEGIN ADC1_Init 0 */
 
 /* USER CODE END ADC1_Init 0 */
 
 ADC_ChannelConfTypeDef sConfig = {0};
 
 /* USER CODE BEGIN ADC1_Init 1 */
 
 /* USER CODE END ADC1_Init 1 */
 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 3;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_14;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_47CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = ADC_REGULAR_RANK_3;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */
 
 /* USER CODE END ADC1_Init 2 */
 
}

TomC
TomCAuthorBest answer
Senior
Jan 28, 2021 1:07 AM UTC

The reason I was unable to change channel correctly and thus read another ADC pin was because I did not specify the "Number of Conversions" as the number of channels I wished to use in the ADC's configuration.