Skip to main content
MSing.1713
Associate III
Nov 4, 2025 12:29 AM UTC
Solved

aci_gatt_write_char_desc() uses undocumented ACI command opcode 0xFD21

Greetings,

There is a post explaining how the aci_gatt_write_char_desc() function should be used to enable notification events for a characteristic that may be notified by the server/peripheral.  The opcode, defined as

rq.ogf = 0x3f;
rq.ocf = 0x121;

is the 16 bit opcode 0xFD21.  The September 2025 release of AN5270 (revision 32) omits this command.

Can we get an update to the AN5270 with an explanation of this command?

Cheers

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Nov 6, 2025 9:13 AM UTC

Hi @MSing.1713 ,

After an internal cross-check with the Wireless team, In fact the latest release aims to improve and simplify the code by avoiding duplicate commands, there is indeed few commands such as: ACI_GATT_READ_CHAR_DESC, ACI_GATT_READ_LONG_CHAR_DESC, ACI_GATT_WRITE_CHAR_DESC and ACI_GATT_WRITE_LONG_CHAR_DESC which can be considered as “replaced” by the existing API (now ending by _VALUE). 

“Replaced” means that an old API has been replaced to a new API (the old API can be used with the ble_legacy.h file, but for new application it's recommended to use the new API).

Concerning the duplication of ACI_GATT_WRITE_WITHOUT_RESP (in 2.6.31 and 2.6.44 sections):
Indeed, we confirm it is a mistake, it is just that the command ACI_GATT_WRITE_WITHOUT_RESP_EXT should be present (and not twice ACI_GATT_WRITE_WITHOUT_RESP). This change will be present in coming new version Rev33.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

4 replies

ST Technical Moderator
Nov 4, 2025 6:17 AM UTC

Hello @MSing.1713 

Thanks for your post.

I am checking this internally with the relevant team to clarify this topic (internal ticket number 221063)
We will provide you an update as soon as possible.

Thanks for your contribution.

(PS: ticket number 221063 is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MSing.1713
Associate III
Nov 4, 2025 6:35 AM UTC

Cool.

I also noticed that there are two opcodes with the same description, or at least as far as I can tell.

2.6.31 ACI_GATT_WRITE_WITHOUT_RESP

2.6.44 ACI_GATT_WRITE_WITHOUT_RESP

There may be a difference somewhere in the description, but I'm not seeing it.

Thoughts?

MSing.1713
Associate III
Nov 4, 2025 10:21 PM UTC

I found a few other anomalies.  These commands are declared in the API.  The following opcodes are present in the firmware implementation, but not in the documentation v32. AN5270.  Amusingly, there are two in the documentation and not declared in code.

ACI_GATT_WRITE_WITHOUT_RESP 0xFD40
ACI_GATT_WRITE_WITH_RESP_EXT 0xFD41

I did not scan the HCI commands, only the ACI extensions.  As far as I can see, these below are the only undocumented commands defined in the sample code.

-------------------------------------------

 

tBleStatus aci_gatt_write_long_char_desc( uint16_t Connection_Handle,
tBleStatus status = 0;
rq.ogf = 0x3f;
rq.ocf = 0x11f;
tBleStatus aci_gatt_read_long_char_desc( uint16_t Connection_Handle,
tBleStatus status = 0;
rq.ogf = 0x3f;
rq.ocf = 0x120;
tBleStatus aci_gatt_write_char_desc( uint16_t Connection_Handle,
tBleStatus status = 0;
rq.ogf = 0x3f;
rq.ocf = 0x121;
tBleStatus aci_gatt_read_char_desc( uint16_t Connection_Handle,
tBleStatus status = 0;
rq.ogf = 0x3f;
rq.ocf = 0x122;

tBleStatus aci_gatt_deny_read( uint16_t Connection_Handle,
tBleStatus status = 0;
rq.ogf = 0x3f;
rq.ocf = 0x12d;

Imen.DBest answer
ST Technical Moderator
Nov 6, 2025 9:13 AM UTC

Hi @MSing.1713 ,

After an internal cross-check with the Wireless team, In fact the latest release aims to improve and simplify the code by avoiding duplicate commands, there is indeed few commands such as: ACI_GATT_READ_CHAR_DESC, ACI_GATT_READ_LONG_CHAR_DESC, ACI_GATT_WRITE_CHAR_DESC and ACI_GATT_WRITE_LONG_CHAR_DESC which can be considered as “replaced” by the existing API (now ending by _VALUE). 

“Replaced” means that an old API has been replaced to a new API (the old API can be used with the ble_legacy.h file, but for new application it's recommended to use the new API).

Concerning the duplication of ACI_GATT_WRITE_WITHOUT_RESP (in 2.6.31 and 2.6.44 sections):
Indeed, we confirm it is a mistake, it is just that the command ACI_GATT_WRITE_WITHOUT_RESP_EXT should be present (and not twice ACI_GATT_WRITE_WITHOUT_RESP). This change will be present in coming new version Rev33.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks