Question
aci_gap_create_connection() never returns on STM32WB5MM
Hello,
I'm using the client/server example with two Nucleo-WB55 kit, it works without issue.
Now I'm working with my own board:
Client : STM32WB5MM module
Server: the same nucleo-WB55 as above
At starting, the client scans and detects the server(with the right BLE address). But during the Connect_Request(), the client never returns from aci_gap_create_connection().
I did a clean configuration from cubeMX and I get exactly the same problem, and I have tried with two differents boards.
I have no idea why there is no return (success or not)...
My BLE stack is 1.18.0
Thank you,
Pierre