Skip to main content
Rob Keck
Associate
Feb 15, 2017 10:27 AM UTC
Question

Accuracy of MSI (Timing problem with LMIC)

Posted on February 15, 2017 at 11:27

Hey there. 

I am experimenting with LoRaWAN (the things network) and the STM32L053C8 discovery board.

I set up my sysclock to MSI 2 MHz and the systick interrupt to count up 10000 times a second (100us ticks). 

This is required by the lmic library to provide accurate timing for 2 receive windows.

The problem is, that both of the receive windows time out every time. So the question is if it's possible that the clock is that inaccurate or maybe i did some wrong in the configuration.

Would be very nice if someone could have a look at my code.

Code is attached as eclipse project.

Thanks in advance.

Kind regards, Rob

#lorawan #sx1276 #clock-hsi-msi-lsi #system-clock #systick #lora
This topic has been closed for replies.