Skip to main content
AMova.2
Associate II
Mar 9, 2023 2:29 PM UTC
Solved

About the LSE Crystall to the STM32WB55

In STM32WB55 the LSF must be 32KHz or it can be others like 42KHz etc. as well?

Thanks.

This topic has been closed for replies.
Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Mar 31, 2023 4:50 PM UTC

Hello,

It is highly recommended to use an LSE crystal at 32 kHz for BLE application.

Best Regards

4 replies

Foued_KH
ST Employee
Mar 9, 2023 2:47 PM UTC

Hello @Community member​ ,

The typical LSE frequency is 32KHz (from STM32WB55 DS)

0693W00000aIaxJQAS.pngFoued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AMova.2
AMova.2Author
Associate II
Mar 9, 2023 5:40 PM UTC

Dear Khalsi,

Thank you for your reply. Yes, I agree that the typical value for the LSE crystal is 32KHz. So, according to the table shown above we can select up to maximum 44.4 KHz for the LSE crystal. If we select 42 KHz for the LSE this would not violet the BLE portion of the STM32WB55RG please?

Thanks,

ALi.

AMova.2
AMova.2Author
Associate II
Mar 9, 2023 6:44 PM UTC

Dear Khalsi,

I did search in the community, and I found a similar type of question,

STM32WB55 custom board and 32Khz crystal

Imen refers to the AN5042 "Application note Precise HSE frequency and startup time tuning for STM32 wireless MCUs". I did check this App and I did not see any information regarding the 32KHz LSE. I am assuming that LSE has no role in the functionality of the BLE portion of the STM32WB55 please. According to your table I can select different frequencies beside 32 KHz as long as I follow the limit.

Please comment.

Thanks for your help.

Remy ISSALYS
Remy ISSALYSBest answer
ST Technical Moderator
Mar 31, 2023 4:50 PM UTC

Hello,

It is highly recommended to use an LSE crystal at 32 kHz for BLE application.

Best Regards