Skip to main content
Associate III
Mar 30, 2026 3:08 AM UTC
Solved

About STM32WBA25 RAM Size for Multiple Functions

Hi

If I develop an application using the STM32WBA25 MCU with BLE, ThreadX, and USBX, is the RAM size sufficient?

Pavel A.
Pavel A.Best answer
Mar 30, 2026 5:20 AM UTC

Eric,

It looks feasible, but actually depends on the application RAM usage, on the compiler (some compilers optimize better) so it's hard to tell. Do you have alternatives?

8 replies

Pavel A.
Mar 30, 2026 3:22 AM UTC

96KB looks like decent amount of RAM  - but RTOSes such as ThreadX require a lot of RAM for thread stacks. So it highly depends on the number of your tasks/threads. 

 

CY_TsaiAuthor
Associate III
Mar 30, 2026 3:32 AM UTC

Hi @Pavel A. ,

Given that my application includes approximately 3 KB of historical data, a CC protocol using the FUSB302B, and a USBX CDC stack requiring at least 12 KB of memory, would you recommend continuing development with the STM32WBA25 series?

 

Sincerely.

Eric

Pavel A.
Pavel A.Best answer
Mar 30, 2026 5:20 AM UTC

Eric,

It looks feasible, but actually depends on the application RAM usage, on the compiler (some compilers optimize better) so it's hard to tell. Do you have alternatives?