Skip to main content
ALomb
Senior
Nov 17, 2020 11:50 AM UTC
Solved

X-NUCLEO-GFX01M1 and NUCLEO-F446RE: External Loader

I'm trying to port the STM32G071 NUCLEO DEMO downloaded via TouchGFX Designer 4.15.0 to the NUCLEO-F446RE.

In order to use the external SPI Flash memory on the X-NUCLEO-GFX01M1 I need the external loder for the STM32F4 processor.

The project downloaded via TouchGFX Designer 4.15.0 provides the external loader MX25L6433F_STM32G071B_NUCLEO.stldr in binary format.

Is it possible to have the external loader project so that it can be adapted to other STM32s (STM32F446 in my case) ?

Or I have to necessarily implement it from scratch, maybe I get started on the MOOC "How to create an external QSPI loader MOOC" ?

This topic has been closed for replies.
ALomb
ALombBest answer
Senior
Nov 18, 2020 4:32 PM UTC

I have implemented the external loader !

If it helps, in addition to the MOOC link, I referenced the following links:

and the demo project in C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoader directory.

Many thanks to @Tilen MAJERLE​ !

Attached the stldr

1 reply

ALomb
ALombAuthorBest answer
Senior
Nov 18, 2020 4:32 PM UTC

I have implemented the external loader !

If it helps, in addition to the MOOC link, I referenced the following links:

and the demo project in C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoader directory.

Many thanks to @Tilen MAJERLE​ !

Attached the stldr