Skip to main content
ST Employee
Mar 14, 2024 12:08 PM UTC
Question

X-CUBE-TOUCHGFX 4.23.2 is out!

TouchGFX 4.23.2 is now out.

Please follow this link to download it.

4.23.2 Release details:

  • Release date: March 14th, 2024

  • Bugfixes in TouchGFX Designer:

    • Fixed a bug where TouchGFX Designer would not close properly
  • Bugfixes in TouchGFX Core:

    • Fixed issue were accessing cached bitmap data could result in unaligned
      memory accesses.

4.23.1 Release details:

  • Release date: January 22nd, 2024

  • Bugfixes in TouchGFX Designer:

    • Fixed TextArea lineheight in canvas not matching with rendered lineheight.
    • Fixed 'tgfx.exe generate' creating new 'touchgfx_backup' everytime it is executed.
    • Fixed opening properties for 'Grid Lines' and 'Labels' on graph widgets enabling and disabling them.
    • Fixed importing Custom Widgets with fonts causing issues.
  • New TouchGFX Core Features:

    • Added methods SwipeContainer::goNextPage() and SwipeContainer::goPreviousPage() to change page with an animation.
  • Bugfixes in TouchGFX Core:

    • Fixed issue where kerning data was sometimes missing for vector fonts.
    • Fixed issue where CacheableContainer could draw outside the invalidated area.
    • Drawing vector fonts on STM32U599/5A9 using GPU2D (NeoChrom) would result in poor anti-aliasing.
    • Fixed Keil library nemagfx_core_release.lib to use lcd class "LCDGPU2D_AXI" instead of "LCDGPU2D" for cortex M7 and M55.
  • New TouchGFX Generator Features:
    • Support for TrustZone applications (STM32L5/STM32U5).
  • Bugfixes in TouchGFX Generator:
    • Having Video Decoding enabled on ThreadX applications would result in compilation errors when using MDKARM.

Note : TouchGFX Designer 4.23.2 MUST be used with STM32CubeMX 6.10.0 or above (link to download STM32CubeMX).

Attention : If X-CUBE-TOUCHGFX 4.23.2 is not available in STM32CubeMX software yet, please navigate to "Help > Manage embedded software packages > STMicroelectronics > X-CUBE-TOUCHGFX". Then click on "From Local ..." and navigate to the x-cube-touchgfx-4-23-2.zip file to install the new pack inside STM32CubeMX.

 

Please also check our Known Issues article.

 

Enjoy this new version ! :)

This topic has been closed for replies.

1 reply

KMacD
Associate
Mar 20, 2024 12:24 AM UTC

Attention : If X-CUBE-TOUCHGFX 4.23.2 is not available in STM32CubeMX software yet, please navigate to "Help > Manage embedded software packages > STMicroelectronics > X-CUBE-TOUCHGFX". Then click on "From Local ..." and navigate to the x-cube-touchgfx-4-23-2.zip file to install the new pack inside STM32CubeMX.

 

Perfect!  much appreciated.