Skip to main content
BRado
Associate II
February 10, 2020
Solved

X-CUBE-TOUCHEGFX v4.13.0 vs STM32L4R9AI

Hello,

Can we, now, generate a STM32L4R9AI project with STM32CubIde including TouchGFX Middelware ?

X-CUBE-TOUCHEGFX v4.13.0 offer this possibility or not yet ?

Tankyou.

This topic has been closed for replies.
Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
February 17, 2020

Hello,

The porting of the STM32L4R9 Discovery Board is currently being done. Hopefully, this will be finished by the end of this week.

I will write another comment to inform you.

20 replies

BRado
BRadoAuthor
Associate II
April 8, 2020

What kind of UI do you want to display ?

  •           ​Only background ( simple Photo).

Is the background of your UI supposed to be white ?

  •          No the bakground is not white

Except the DSI to LTDC-RGB change, did you change something else ?

  • Except DSI to RGB565 no change is added.
Alexandre RENOUX
Visitor II
April 8, 2020

Do you confirm using the v3.0.0 (TouchGFX Generator) Application template for the L4R9-EVAL ?

Because the L4R9-EVAL AT only supports 24 bits depth color. The 16 bits support is not done because the screen that is supposed to be on this board is 24 bits.

In any case, for some boards the 16 bits depth color is not supported while it should, and these are among the tasks to be done.

I will try to give you some feedback in the near future regarding that.

To summarize, the bit depth color might be the issue. In the meantime, you can have a look at the F469-EVAL or DISCO AT to understand how the switch between 16 bits and 24 bits is performed.

/Alexandre

BRado
BRadoAuthor
Associate II
April 8, 2020

 ​Yes, I m using the v3.0.0 (TouchGFX Generator) Application template for the L4R9-EVAL. So we modified the L4R9-EVAL to support 16Bits

the LCD used is a custom one.

I inform you that when I build the project by my self, All work and the UI is running ... but whith TouchGFX Generator I have the problem.

I want generat the project throught  STM32CubIDE to benifit of MCU configuration facility.

RBI

Alexandre RENOUX
Visitor II
April 8, 2020

So if I understand correctly you have one project that works with your custom LCD and does not use the latest version with TouchGFX Generator (v3.0.0) and when you try to make the same project but using Generator you encountered an issue on the display ? And you have no idea what is the difference between these 2 projects, is that the current status ?

/Alexandre

BRado
BRadoAuthor
Associate II
April 8, 2020

​Exactly, this is the current status.

BRado
BRadoAuthor
Associate II
June 2, 2020

Any adea to resolve my problem ?

Thank's

Alexandre RENOUX
Visitor II
June 2, 2020

Hi,

Sorry, a lot of other things came up and I was not able to look at it.

In a previous message you mentioned "I inform you that when I build the project by my self, All work and the UI is running ... but whith TouchGFX Generator I have the problem". What do you mean you built your project by yourself, can you give more details on your procedure ?

Then you say "I want generate the project through STM32CubIDE to benifit of MCU configuration facility.". We haven't tested using CubeMX inside CubeIDE so I suggest you to avoid doing it. Set the parameters of your project in CubeMX, generate code, then generate code from TouchGFX Designer and finally open CubeIDE to build and download the binary file into the board.

Have you tried debugging and see where it stops ? If yes, could you provide information about it ?

It's difficult to find the cause of your problem quickly because I cannot test it myself, you are using an screen we never tested and you changed from DSI to LTDC on the L4R9 which is something we haven't tested so far.

/Alexandre