Skip to main content
Associate
Jul 16, 2025 11:10 AM UTC
Solved

Wildcard text works perfectly in TouchGFX simulator but not when flashed to board!

I’m working on a TouchGFX project with a dropdown menu. When I select an option, the selected text is shown in a TextArea using a wildcard buffer (selectedTextBuffer).

In the TouchGFX Simulator, the full string displays correctly. But on the actual STM32 board, only the first letter (e.g., just "M") is visible.

I've already tried the following:

  • Set the buffer size in Designer to 32

  • Confirmed that all characters are included in the font's wildcard character set

  • Verified that invalidate() is called after updating text

  • Rebuilt assets and fully flashed the board

Despite all this, the board still only shows the first letter.

Setup:

  • MCU: STM32H7 (STM32H750-DK)

  • TouchGFX version: 4.25.0

  • TextArea uses selectedTextBuffer as wildcard

This topic has been closed for replies.
BTKottary27Best answer
Associate
Jul 23, 2025 7:18 PM UTC

If you changed the text displayed to something else, "Test", does it always show only the first letter? 

Yes

If you add more M's (keep them capitalized), will it display them?

No, only first letter

Are you using Typed text or creating the text programmatically with snprintf? 

creating using snprintf

If you don't use a wildcard but simply place text in there will it display correctly?

Yes It does.

 

Anyways I used the textID of the buttons in the dropdown menu to set to my desired wildcard text. It worked for me. 

Thanks!

 

6 replies

ST Employee
Jul 17, 2025 11:02 AM UTC

Hello @BTKottary27,

Your text area is big enough to show all the characters ? Try to call resizeToCurrentText() TextArea | TouchGFX Documentation.

BR,

Louis BOUDOST Software Engineer | TouchGFX
Associate
Jul 17, 2025 12:17 PM UTC

tried resizeToCurrentText() , No changes. It works perfectly fine for me in simulator but not on board!

ST Employee
Jul 22, 2025 8:22 AM UTC

Hello @BTKottary27 

You can try to debug the target, check what value is passed to the textArea and if the invalidation is made correctly.

BR,

Louis BOUDOST Software Engineer | TouchGFX
jchernus-fikst
Senior
Jul 23, 2025 2:59 PM UTC

Were you able to resolve this?

If you changed the text displayed to something else, "Test", does it always show only the first letter? If you add more M's (keep them capitalized), will it display them? Are you using Typed text or creating the text programmatically with snprintf? If you don't use a wildcard but simply place text in there will it display correctly?

BTKottary27AuthorBest answer
Associate
Jul 23, 2025 7:18 PM UTC

If you changed the text displayed to something else, "Test", does it always show only the first letter? 

Yes

If you add more M's (keep them capitalized), will it display them?

No, only first letter

Are you using Typed text or creating the text programmatically with snprintf? 

creating using snprintf

If you don't use a wildcard but simply place text in there will it display correctly?

Yes It does.

 

Anyways I used the textID of the buttons in the dropdown menu to set to my desired wildcard text. It worked for me. 

Thanks!

 

jchernus-fikst
Senior
Jul 23, 2025 8:28 PM UTC

Great! That's probably the better way to go as it supports localization (different languages, formatting).