Skip to main content
LLiao.1
Associate II
Nov 18, 2020 9:12 AM UTC
Question

why the touch point and the displayed position are exactly opposite?

Hello, 

I used the SMT32F429i-DISC1 and TouchGFX follow the user guide

coding, why the touch point and the displayed position are exactly opposite?

For example, if my button is on the far left, I have to press the far right position of panel to respond?

Thanks

This topic has been closed for replies.

15 replies

Martin KJELDSEN
Principal III
Aug 11, 2021 8:27 AM UTC

I'll ask with the team responsible for ATs if they're aware of any current issues with the new 429-disc board.

OHenr.1
Visitor II
Aug 11, 2021 3:51 PM UTC

Hello,

I got the blue board MB1075-F429I-E01

I used TouchGFXdesigner 4.14.0

I upgraded now to 4.16.1 , This version works now with my board, it has a different board selector and produces the right code.

The compiled binary firmware file from the board support page does not work with my board.

/Oliver

Martin KJELDSEN
Principal III
Aug 12, 2021 10:15 AM UTC

Thanks for the feedback, @OHenr.1​ 

MPasc.3
Visitor II
Feb 23, 2022 2:13 PM UTC

Hello guys,

Did you guys find a solution for this problem? I am using TouchGFX 4.18.1 and the displayed positions are still reversed.

Thank you!

AAdam.2
Visitor II
Jul 29, 2022 6:59 PM UTC

Not sure if this helps anyone, but I had this issue when I choose the wrong stm32f429 variant.. D1 instead of E1.