Skip to main content
CBald
Associate III
June 2, 2020
Question

Why is there no 8 bpp option for GFXMMU?

My framebuffer is 8 bpp in L8 format, but under GFXMMU > LUT Configuration > Display BPP, there is no 8 bpp option? Am I missing something? Considering the LTDC supports 8 bpp framebuffers, this should definitely be an option.

Currently running the latest CubeIDE with whatever CubeMX is built in.

This topic has been closed for replies.

4 replies

TDK
June 2, 2020

Some chips don't have enough pins to support all modes. What chip are you using?

"If you feel a post has answered your question, please click ""Accept as Solution""."
CBald
CBaldAuthor
Associate III
June 2, 2020

Pretty sure that's not it, but for reference I'm using an STM32L4R9AI with DSI interface (so pins aren't the issue)

TDK
June 2, 2020

You're right, it's unlikely to be that. Probably just one of those things where even though the underlying hardware supports it, the HAL/CubeMX infrastructure isn't set up to support it yet. L4+ is pretty new.

"If you feel a post has answered your question, please click ""Accept as Solution""."
CBald
CBaldAuthor
Associate III
June 2, 2020

L4+ and the GFXMMU have been around for 3 years now (date code on my eval board is 8th week, 2017)... I'd expect them to have this sorted out by now. They have 16, 24, and 32bpp options, I just don't understand why 8bpp isn't there. Should be trivial to add. Is there a place I can feature request this?