Skip to main content
Sammalisto.Pauli
Associate II
January 24, 2022
Solved

Why are European characters wrong in STemWin.

I opened and build a STM32F429 STemWin Hello world application in the latest STM32Cube Repository. All works fine, but if I add/change some European letters to the text, eg. Ä, Ö and Å are wrong. They are printed something like A+tilde and a "reverse" P (Word's paragraph mark). I have some other old "green field" STemWin applications that worked then ok, but have now the same problem. Is there anything I can do to correct the behavior?

I am using W10, STM32CubeIde and TrueStudio. The old applications were made by TrueStudio. The problem is in both frameworks.

Where can I get information about these new libraries, what is what. The same error is now with old and new libraries.

This topic has been closed for replies.
PCu1
PCu1Best answer
Senior
January 25, 2022

Hello,

Moving from Atollic to CubeIDE gave me some issues for STemwin.

The Codepage of the file is not the same and my comments and STemwin texts(accented characters) in the source code appeared like you mention.

==> my solution

I first checked that CubeIDE C files are in UT8.

After that I replaced wrong character in source code.

Finally I added this line in after GUI_init():

GUI_UC_SetEncodeUTF8();

Hope this help.

Pierre

2 replies

PCu1
PCu1Best answer
Senior
January 25, 2022

Hello,

Moving from Atollic to CubeIDE gave me some issues for STemwin.

The Codepage of the file is not the same and my comments and STemwin texts(accented characters) in the source code appeared like you mention.

==> my solution

I first checked that CubeIDE C files are in UT8.

After that I replaced wrong character in source code.

Finally I added this line in after GUI_init():

GUI_UC_SetEncodeUTF8();

Hope this help.

Pierre

Sammalisto.Pauli
Associate II
January 26, 2022

Thank you Pierre, that helped a lot, all works now fine.

I was struggling with encodings and character sets in the 80's, but it did not occur to me, that I need now unicode, especially when the characters are in ISO 8859 character set in manual page 250.